1 Harmony 3 Driver and System Service Application Examples for PIC32MZ EF Family
The following applications are provided to demonstrate the typical or interesting usage models of one or more drivers and system services.
| Name | Description |
|---|---|
| Console Debug System Service using UART | This example application demonstrates the UART based console and debug system service |
| Console Debug System Service using USB | This example application demonstrates the USB based console and debug system service |
| FAT Filesystem using NVM and SDSPI Media | This application shows an example of using the MPLAB Harmony File System to access files across multiple media (NVM, SDSPI) |
| FAT Filesystem using NVM and SST26 Media | This application shows an example of using the MPLAB Harmony File System to access multiple files across multiple media (NVM, SQI FLASH) |
| FAT Filesystem using NVM Media | This application shows an example of implementing a FAT disk in the device internal Flash memory |
| FAT Filesystem using SDSPI Media | This application shows an example of using the MPLAB Harmony File System to access and modify the contents of a SD card using the SDSPI driver and the SPI PLIB |
| FAT Filesystem using SST26 Media | This application shows an example of using the MPLAB Harmony File System to access SQI based SST26 flash media |
| FreeRTOS Basic | This example application demonstrates context switching between four tasks of different priorities. Two tasks run periodically while the other two tasks are event driven |
| FreeRTOS Task Notification | This example application is to illustrate the FreeRTOS Task Notification feature which is used as a light weight binary semaphore |
| Memory Driver Asynchronous - NVM SST26 Read Write | This example application shows how to use the Memory driver in asynchronous mode to perform block operations on the NVM and the SST26 media’s |
| Memory Driver Synchronous - NVM SST26 Read Write | This example application shows how to use the Memory driver in synchronous mode to perform block operations on the NVM and the SST26 media’s. |
| MPFS Filesystem using NVM Media | This application shows an example of implementing a MPFS disk in device Internal Flash memory |
| SDSPI Driver Synchronous - SDSPI Read Write | This example application shows how to use the SDSPI driver in synchronous mode to perform block operations on the SD Card Media |
| SPI Driver Asynchronous - Self Loopback Multi Client | This example demonstrates how to use the SPI driver in asynchronous mode to achieve self-loop back between multiple clients |
| SPI Driver Synchronous - Self Loopback Multi Client | This example demonstrates how to use the SPI driver in synchronous mode to achieve self-loop back between multiple clients in RTOS environment |
| SQI Flash SST26 Driver - SST26 SQI Read Write | This example application shows how to use the SST26 driver to perform block operations on the On-Board SST26 Flash memory in Quad IO mode |
| Time System Service Multi-client | This example application demonstrates the multi-client system timer functionality |
| USART Driver Asynchronous - USART Echo | This example echoes the received characters over the console using the USART driver in asynchronous mode |
| USART Driver Synchronous - USART Echo | This example echoes the received characters over the console using the USART driver in synchronous mode |