| 1. | M8PD-11560 | Renamed APIs for consistency and better alignment |
| 2. | M8PD-11558 | Hard-coded hex values are replaced with DFP defined macros |
| 3. | M8PD-11557 | Improved code quality by reducing MISRA violations |
| 4. | M8PD-10998 | Display conversion time in user interface |
| 5. | M8PD-9381 | Fixed issue where the Pin Grid View did not display a row for differential channels in Differential mode |
| 6. | M8PD-8665 | Users can now select the ADC channel using custom pin names in addition to the actual channel names |
| 7. | M8PD-7114 | Fixed an issue where enabling the Result Ready Interrupt caused the program to enter a spin lock within the GetConversion API |
| 8. | M8PD-5249 | Selecting an analog pin in Easy View now correctly highlights the corresponding hardware pin in Pin Grid View |
| 9. | M8PD-5240 | Fixed issue where setting the Lower Threshold from Easy View did not update the actual register value |
| 10. | M8PD-5189 | Fixed issue where the sample rate calculation was incorrect |
| 11. | M8PD-5146 | Updated firmware with new APIs and enhancements to existing functionalities |
| 12. | M8PD-5132 | Updated user interface for a more intuitive and user-friendly experience |