1.8 SPI EEPROM AT25 Driver - EEPROM Read Write
This example application shows how to use the AT25 driver to perform read and write operations on AT25 series of EEPROM.
Description
This example uses the AT25 driver to communicate with the SPI based AT25 series of external EEPROMs to perform write and read operations in Bare-Metal environment.
Downloading and Building the Application
To clone or download this application from Github, go to the main page of this repository and then click Clone button to clone this repository or download as zip file. This content can also be downloaded using content manager by following these instructions.
Path of the application within the repository is apps/driver/spi_eeprom/at25/at25_eeprom_read_write/firmware.
To build the application, refer to the following table and open the project using its IDE.
| Project Name | Description |
|---|---|
| sam_a7g5_ek.X | MPLABX project for SAMA7G54 Evaluation Kit |
Setting Up AT91Bootstrap loader
To load the application binary onto the target device, we need to use at91bootstrap loader. Refer to the at91bootstrap loader documentation for details on how to configure, build and run bootstrap loader project and use it to bootstrap the application binaries.
Setting Up the Hardware
The following table shows the target hardware for the application projects.
| Project Name | Description |
|---|---|
| sam_a7g5_ek.X | SAMA7G54 Evaluation Kit |
Setting Up SAMA7G54 Evaluation Kit
- EEPROM 4 Click board
- Install an EEPROM 4 Click board on to the mikroBUS1 connector
- Connect the USB port J7 on board to the computer using a micro USB cable (to power the board)
- Connect the USB port J24 on board to the computer using a micro USB cable (to enable debug com port)
Running the Application
- Build the application using its IDE.
- The LED is turned ON when the value read from EEPROM matches with the written data.
| Board | LED Name |
|---|---|
| SAMA7G54 Evaluation Kit | RGB_LED (Blue) |