1.5.4.14 AL_EVENT_IND_CALLBACK Typedef
C
typedef void ( *AL_EVENT_IND_CALLBACK )( AL_EVENT_IND_PARAMS *eventParams );
Summary
Pointer to a Meters And More AL module Event Indication Function Pointer.
Description
This data type defines the required function signature for the Meters And More AL module Event Indication callback function. A client must register a pointer using the callback register function whose function signature (parameter and return value types) match the types specified by this function pointer in order to receive related event callbacks from the module.
Parameters
| Param | Description |
|---|---|
|
eventParams |
Pointer to the object containing any data necessary to process the Event Indication primitive. See AL_EVENT_IND_PARAMS Struct |
Returns
None.
Example
void APP_MyEventIndEventHandler( DLL_EVENT_IND_PARAMS *eventParams )
{
if (eventParams->eventId == AL_EVENT_ID_MAC_ACA){
/* Timeout coming from a remote node */
}
}
Remarks
This Callback is only generated in Master Node. There is no need to handle it on Slave Nodes.