1 Harmony 3 Driver, System Services and RTOS Application Examples for PIC32CX-BZ2 and WBZ451 Family

The following applications are provided to demonstrate the typical or interesting usage models of one or more drivers, system services and RTOS.
NameDescription
Console Debug System Service using UARTThis example application demonstrates the UART based console and debug system service
FAT File System using NVM MediaThis application shows an example of implementing a FAT disk in the device internal Flash memory
FAT File System using SD Card MediaThis application shows an example of using the MPLAB Harmony File System to access and modify the contents of a SD card using the SDSPI driver and the SPI PLIB
FreeRTOS BasicThis example application demonstrates context switching between four tasks of different priorities. Two tasks run periodically while the other two tasks are event driven
I2C Driver Asynchronous - I2C EEPROMThis example application shows how to use the I2C driver in asynchronous mode to perform operations on the EEPROM
SPI Driver Asynchronous - Self Loopback Multi ClientThis example demonstrates how to use the SPI driver in asynchronous mode to achieve self-loop back between multiple clients
Time System Service Multi-clientThis example application demonstrates the multi-client system timer functionality
USART Driver Asynchronous - USART EchoThis example echoes the received characters over the console using the USART driver in asynchronous mode
USART Driver Synchronous - USART EchoThis example echoes the received characters over the console using the USART driver in synchronous mode