3.1 Industrial Device Mission Profile Example
The values shown in the section Industrial Device Lifetime Estimates are based on estimates for an always-on device (100% up time). However, all applications are not up 100% of the time and may switch from one operating point (TJ, VDD) to another. Such considerations must be taken into account when estimating lifetime.
To estimate a specific mission profile, use the following tables and examples.
Table 3-2, built from applicable product qualification, temperature and voltage aging acceleration values, lists the A, B, C and D operating points referred to in the example below.
| TJ | DR(TJ) | Mission Profile Example |
|---|---|---|
| TJ°C < 25°C | 938 | |
| 30 | 598 | |
| 35 | 387 | |
| 40 | 254 | |
| 45 | 169 | |
| 50 | 114 | A |
| 55 | 77.7 | |
| 60 | 53.6 | |
| 65 | 37.3 | |
| 70 | 26.3 | B |
| 75 | 18.7 | |
| 80 | 13.5 | |
| 85 | 9.8 | |
| 90 | 7.1 | |
| 95 | 5.3 | |
| 100 | 3.9 | C |
| 105 | 2.9 | |
| 110 | 2.2 | |
| 115 | 1.7 | |
| 120 | 1.3 | |
| 125 | 1 | D |
- A target lifetime: PoHMP_TARGET
- 4 operating points (VDD, TJ)
- A usage percentage in each operating point
PoHMP_TARGET = 60,000 Hrs
| MP | U% | PoH(TJ, VDD) | TJ °C | VDD (V) | DR(TJ) | VAF | PoH(125°C, 1.15V) | Comment |
|---|---|---|---|---|---|---|---|---|
| A | 25 | 15000 | 50 | 1.05 | 114 | 2.72 | 48 | 15000 / 114 / 2.72 = 48 |
| B | 25 | 15000 | 70 | 1.15 | 26.3 | 1.00 | 570 | 15000 / 26.3 / 1 = 570 |
| C | 25 | 15000 | 100 | 1.05 | 4 | 2.72 | 1406 | 15000 / 4 / 2.72 = 1406 |
| D | 25 | 15000 | 125 | 1.25 | 1 | 0.368 | 40774 | 15000 / 1 / 1 = 40774 |
| PoHMP(125°C, 1.15V) = | 42799 | |||||||
The PoH(125°C, 1.15V) column is computed for each line of the mission profile by derating PoH(TJ, VDD) with DR(TJ) and VAF (temperature and voltage derating). Computation results are then summed up into a single value.
- If the computed PoHMP(125°C, 1.15V) is greater than PoHQ(125°C, 1.15V), then the required PoHMP_TARGET exceeds the device lifetime emulated during the HTOL tests, as in this example. In such a case, the mission profile must be reviewed.
- Conversely, if PoHMP(125°C, 1.15V) is less than PoHQ(125°C, 1.15V), then the mission profile MP is covered by the HTOL tests.
As explained above, PoHMP_TARGET = 60 kHrs cannot be reached with the example mission profile MP. However, it is interesting to estimate the Power-on Hours with such a mission profile, PoHMP_EST. See the applicable formula in Table 2-1 and its application in the following table.
| Result | Value in Hours | Comment |
|---|---|---|
| PoHMP_EST | 41463 | 60,000 * 29576 / 42799 |