4.1 Automotive Device Mission Profile Example
The values shown in Automotive Device Lifetime Estimates are based on estimates for an always-on device (100% up time). However, all applications are not up 100% of the time and may switch from one operating point (VDD, TJ) to another. Such considerations must be taken into account when estimating lifetime.
To estimate a specific mission profile, use the following tables and examples.
Table 4-2, built from applicable product qualification, temperature and voltage aging acceleration values, lists the A, B, C, D, E and F operating points referred to in the example below.
| TJ | DR(TJ) | Mission Profile Example |
|---|---|---|
| TJ°C < 25°C | 937.50 | A |
| 30 | 598.14 | |
| 35 | 387.23 | |
| 40 | 254.20 | |
| 45 | 169.09 | |
| 50 | 113.90 | |
| 55 | 77.66 | |
| 60 | 53.56 | |
| 65 | 37.35 | |
| 70 | 26.32 | B |
| 75 | 18.73 | |
| 80 | 13.46 | |
| 85 | 9.76 | C |
| 90 | 7.15 | |
| 95 | 5.27 | |
| 100 | 3.92 | D |
| 105 | 2.94 | |
| 110 | 2.22 | |
| 115 | 1.69 | E |
| 120 | 1.30 | |
| 125 | 1 | F |
- A target lifetime: PoHMP_TARGET
- 6 operating points (VDD, TJ)
- A usage percentage in each operating point
PoHMP_TARGET = 20,000 Hrs
| MP | U% | PoH(TJ, VDD) | TJ °C | VDD (V) | DR(TJ) | VAF | PoH(125°C, 1.15V) | Comment |
|---|---|---|---|---|---|---|---|---|
| A | 6 | 1200 | -40 | 1.15 | 938 | 1 | 1.28 | 1200 / 938 / 1 = 1.28 |
| B | 25 | 5000 | 70 | 1.15 | 26.3 | 1 | 190 | 5000 / 26.3 / 1 = 190 |
| C | 25 | 5000 | 85 | 1.15 | 9.76 | 1 | 512 | 5000 / 9.76 / 1 = 512 |
| D | 25 | 5000 | 100 | 1.15 | 4 | 1 | 1274.4 | 5000 / 4 / 1 = 1274 |
| E | 14 | 2800 | 115 | 1.15 | 2 | 1 | 1655.3 | 2800 / 2 / 1 = 1655 |
| F | 5 | 1000 | 125 | 1.15 | 1 | 1 | 1000 | 1000 / 1 / 1 = 1000 |
| PoHMP(125°C, 1.15V) = | 4633 | |||||||
The PoH(125°C, 1.15V) column is computed for each line of the mission profile by derating PoH(TJ, VDD) with DR(TJ) and VAF (temperature and voltage derating). Computation results are then summed up into a single value.
- If the computed PoHMP(125°C, 1.15V) is greater than PoHQ(125°C, 1.15V), then the required PoHMP_TARGET exceeds the device lifetime emulated during the HTOL tests. In such a case, the mission profile must be reviewed.
- Conversely, if PoHMP(125°C, 1.15V) is less than PoHQ(125°C, 1.15V), as in this example, then the mission profile MP is covered by the HTOL tests.
As explained above, PoHMP_TARGET = 20 kHrs is reached with the example mission profile MP. However, it is interesting to estimate the Power-on Hours with such a mission profile, PoHMP_EST. See the applicable formula in Table 2-1 and its application in the following table.
| Result | Value in Hours | Comment |
|---|---|---|
| PoHMP_EST | 24748 | 20000 * 5733 / 4633 |