4 What's New?
v4.1.0
Features:
- Added Support for PIC16[L]F184xx, PIC16F131xx, PIC18FxxQ24 and Additional variants of PIC16F171xx devices.
- Added feature to support the configuration of X and Y Lines to enable the user to customize the Matrix view.
- Updated ATTiny161x and ATTiny321x acquisition libraries to version 1.5.
Improvements:
- Migrated from pins-standard module to pins-interface.
- Improved Validation during the creation of new sensors.
- Added restriction to prevent the multiplexing of unsupported lines in the matrix view.
Bug Fixes:
- Added fix for CSD being set as a higher value than 999.
- Added fix for sensors getting hidden during reopening of matrix in mutual-cap multiplexed lines.
- Added fix for lump option being enabled for unsupported devices.
- Added fix for compilation failure when debounce count value is modified.
- Added fix for touch tune data streaming issue when larger data is sent/received.
- Added fix for drivenshield plus code compilation issue in PIC18FxxQ8x devices.
v4.0.0
Features:
- Added Support for PTG based touch Acquisition for dsPIC33CK devices.
Improvements:
- Improved Matrix View for Mutual Capacitance pin assignment
- Added option to update all parameters of same category in sensor parameters table.
- Provision to remove warnings and hints generated by Touch Configurator is added.
- Improved Horizontal Scrollbar visibility.
- Added Clock/Timer inputs in Touch Configurator to input the user loaded modules in UI.
Bug Fixes:
- Added fix for PIC16F18877 compilation issue.
- Added fix sensor not getting added for Q83/Q84 PIC devices.
- Calibration capacitance Interpretation in Datavisualizer is fixed for ATtiny devices.
Important Notes:
- If Timer's custom name is changed from default, then compilation error occurs in touch.c file.
- For AVR devices, CPU clock has to be manually populated in to Touch Configurator. Otherwise Prescaler value used for PTC may not be correct.
v3.5.1
- Bug Fixes and Improvements:
- GAIN and Pre-scaler values are fixed in Configurator for ATmega devices.
- Fixed the bug to edit CSD parameter in Configurator.
- Fixed the bug to load old AVR projects.
- Fixed bug in updating Node parameters properly for Tiny devices in Touch Tune (bidirectional) part of Datavisualizer (Needs MPLAB Touch plugin 2.2.1 as dependency).
- Low power detect threshold parameter is hidden for Software based Low power as it is not applicable.
- Touch_example.c file includes pins header file.
v3.5.0
- Added lump and low power feature support for AVR and PIC devices.
- Added Touch Configurator support for ATmega32(4|8)PB devices.
- Bug fixes and UI improvements.
v3.4.2
- Added fix for AVRDA and ATtiny device compilations error when two-way tuning is enabled.
v3.4.1
- Added fix for AVR and Tiny devices getting error during generation
v3.4.0
- Added Touch Configurator support for dsPIC33CK device families.
- Added future support for PIC18FxxQ20 devices.
- Added touch ADC support for PIC16F1(71/81)xxx devices.
- Added fix for PIC18FxxQ71 device's pins not getting populated in the pins grid view for touch.
- Added fix for compenstaion capacitance (CC) value for self-capacitance technology not being updated properly for ATtiny devices.
- Added fix for input buffer being disabled for PTC Pins.
- Bug fixes and UI improvements.
v3.3.0
-
Touch Configurator support for ATtiny.
-
Added one-touch and two-touch Surface for Self-cap (Mutual-cap will be supported in next release).
- Added Gesture Support.
- Scan Rate control feature is added for PIC devices.
- Improved the Driven Shield feature for user to enable/disable either Driven Shield (or) Driven Shield+ or both for better control .
- Added notification icon within touch configurator to highlight touch related hints, warnings and messages.
- Added fix for not being able to select multiple sensors.
- Added fix for Touch files generation failure when driven shield is enabled.
- Added fix for PIC16F180xx devices not getting loaded.
- Fixed same pins getting generated multiple times in the signal matrix.
- Updated Touch Library to support latest UART libraries.
- Added fix for AVR devices not getting loaded when touch is added.
- Added Button, Slider Wheel sensor support for newly supported devices (Check Supported Devices and Families).
- Added support for two-way Data Streamer protocol through UART communication for both supported AVR and PIC devices (Note: Update to the latest MPLAB touch Plugin v1.0.1).
- Added example .c and .h files during generation of touch files.
- Updated Readme.md content
- Added support for the remaining AVRxxDAxx devices
- Initial release - Touch Library in MCC Melody
- Button, slider and wheels project creation is supported