1.3 Demo Applications
2 demo applications have been developed to guide customers in creating or adding functionality to their own applications.
Smart Energy Demo Meter Application: an example of metering application using the Microchip metrology library with the PIC32CXMTx-DB demonstration kits. The PIC32CXMTx The Demo Meter application runs in the core 0 while the metrology library is running independently in the core 1.
Smart Energy Demo Dual Core Applications: an example showing how to run and communicate 2 separate applications independently on both cores of a PIC32CXMTSH dual core device.
Boards Overview
The following pictures show a global overview of the boards. For a detailed description, refer to the PIC32CXMTSHDB HW User Guide and the PIC32CXMTCDB HW User Guide:


Unpacking the Kit
The Demonstration Kit includes the following:
One PIC32CXMTSH-DB or PIC32CMXMTC-DB board mounted in a protective enclosure.
One Micro A/B-type USB cable.
One ARM-JTAG-20-10 adapter.
One Power Supply adapter (AC/DC) 12vDC, multi-country.
Note: The meter base and the current sensors are not included in the kit.