Once PIC32CXMTG-EK boards are programmed, follow these steps:
Switch the boards off
Connect a PL460-EK to the Xplained expansion port on each of PIC32CXMTG-EK boards
Interconnect PLC Outputs of both PL460-EK boards
Power up PL460-EK boards
Power up PIC32CXMTG-EK boards
The demo application on both boards sends PLC frames randomly.
Each transmitted frame is received by the other board, and this event is indicated by blinking the Blue LED on the PIC32CXMTG-EK board.
The following figure shows the result of the demo running on a set of (PIC32CXMTG-EK + PL460-EK) boards:
Figure . Running Demo App