1.3 Demo Applications
A demo application has been developed to guide customers in creating or adding functionality to their own applications.
- Smart Energy Demo Dual Core Applications: an example showing how to run and communicate 2 separate applications independently on both cores of a PIC32CXMTSH dual core device.
Boards Overview
The following pictures show a global overview of the boards. For a detailed description, refer to the PIC32CXMTSHDB HW User Guide and the PIC32CXMTCDB HW User Guide:


Unpacking the Kit
The Demonstration Kit includes the following:
- One PIC32CXMTSH-DB or PIC32CMXMTC-DB board mounted in a protective enclosure.
- One Micro A/B-type USB cable.
- One ARM-JTAG-20-10 adapter.
- One Power Supply adapter (AC/DC) 12vDC, multi-country.
Note: The meter base and the current sensors are not included in the kit.