1.3 Demo Applications
A demo application has been developed to guide customers in creating or adding functionality to their own applications.
Smart Energy Demo Dual Core Applications: an example showing how to run and communicate 2 separate applications independently on both cores of a PIC32CXMTSH dual core device.
PIC32CXMTSH-DB Board Overview
The following picture shows a global overview of the board. For a detailed description, refer to the PIC32CXMTSH-DB HW User Guide (DS50003024).
Unpacking the Kit
The Demonstration Kit includes the following:
- One PIC32CXMTSH-DB board mounted in a protective enclosure
- One Micro A/B-type USB cable
- One ARM-JTAG-20-10 adapter
- One Power Supply adapter (AC/DC) 12V DC, multi-country
Note: The meter base and the current sensors are not included in
the kit.