8.2 Inductor Selection and Slope Compensation
To select the best inductor for the application, the following factors must be considered: inductance value, RMS rated current, saturation current and DC Resistance (DCR).
The inductance value is critical to correctly operate the MCP16364/5/6. For stable current loop operation where duty cycle is above 50%, slope compensation is internally added according to the output voltage and the input-output voltage ratio.
For the proper amount of slope compensation, it is recommended to keep the inductor down-slope current constant by varying the inductance with VOUT.
VOUT | LSTANDARD |
---|---|
2.0V | 2.2 µH |
3.3V | 3.9 µH |
5.0V | 5.6 µH |
12V | 15 µH |
15V | 15 µH |
The inductor RMS current represents the current at which the inductor’s temperature rises by +20°C to +40°C, depending on the manufacturer. For the inductor saturation current, it represents the peak current where the inductor exhibits a loss of inductance value between 10% and 30%, depending on the manufacturer. For proper operation, ensure that the nominal and peak currents of the application are well within the permissible current ratings of the inductor.
The peak inductor current can be calculated with Equation 8-2:
Where:
IOUT | = | Nominal output current |
VOUT | = | Output voltage |
VIN | = | Input voltage |
fSW | = | Switching frequency |
L | = | Inductance value |
When choosing the inductor, sufficient design margin must be taken into account such that the inductor does not enter deep saturation. Overcurrent situations must also be taken into account, especially at very high input voltages where the inductor current can increase very rapidly.