8.9 PCB Layout Information

Good printed circuit board layout techniques are important to any switching circuitry, and switch mode power supplies are no different. When wiring the switching high-current paths, short and wide traces must be used. Therefore, it is important that the input and output capacitors be placed as close as possible to the MCP16364/5/6 to minimize the loop area.

The feedback resistors and feedback signal must be routed away from the switching node and the switching current loop. When possible, using ground planes and traces is recommended to help shield the feedback signal and minimize noise and magnetic interference.

A good MCP16364/5/6 layout starts with CIN placement. CIN supplies current to the input of the circuit when the switch is turned on. In addition to supplying high-frequency switch current, CIN also provides a stable voltage source for the internal MCP16364/5/6 circuitry. Unstable PWM operation can result if there are excessive transients or ringing on the VIN pin of the MCP16364/5/6 device. A ground plane on the bottom of the board provides a low resistive and inductive path for the return current. The next priority in placement is the freewheeling current loop formed by the Schottky Diode, COUT and L, while strategically placing the COUT return close to ther CIN return. Next, the bootstrap capacitor must be placed between the boost pin and the switch node pin, SW. RTOP and RBOT are routed away from the switch node, so noise is not coupled into the high-impedance FB input.