1.22 RSWDT Timeout
This example shows how to generate a RSWDT reset by emulating a deadlock.
Description
This example demonstrates the usage of Reinforced Safety Watchdog Timer to avoid system deadlock. The simplest way to emulate a deadlock is to wait in an infinite loop. The application enters such an infinite loop when the switch is pressed. As a result the RSWDT counter is not cleared within a bounded time configured using MHC. The RSWDT peripheral will trigger a system reset as the counter exceeds the specified time band.
Downloading and Building the Application
To clone or download this application from Github, go to the main page of this repository and then click Clone button to clone this repository or download as zip file. This content can also be downloaded using content manager by following these instructions.
Path of the application within the repository is apps/rswdt/rswdt_timeout/firmware.
To build the application, refer to the following table and open the project using its IDE.
Project Name | Description |
---|---|
sam_e70_xult.X | MPLABX project for SAM E70 Xplained Ultra Evaluation Kit |
sam_v71_xult.X | MPLABX project for SAM V71 Xplained Ultra Evaluation Kit |
Setting Up the Hardware
The following table shows the target hardware for the application projects.
Project Name | Description |
---|---|
sam_e70_xult.X | SAM E70 Xplained Ultra Evaluation Kit |
sam_v71_xult.X | SAM V71 Xplained Ultra Evaluation Kit |
Setting Up SAM E70 Xplained Ultra Evaluation Kit
- Connect the Debug USB port on the board to the computer using a micro USB cable
Setting Up SAM V71 Xplained Ultra Evaluation Kit
- Connect the Debug USB port on the board to the computer using a micro USB cable
Running the Application
- Open the Terminal application (Ex.:Tera term) on the computer
- Connect to the EDBG Virtual COM port and configure the serial settings as
follows:
- Baud : 115200
- Data : 8 Bits
- Parity : None
- Stop : 1 Bit
- Flow Control : None
- Build and Program the application project using its IDE
- The console displays the following message
- Press the switch to put the system in a deadlock
- LED should stop blinking and the console should print the following message
- RSWDT will reset the device in four seconds and the demonstration should restart
Board | Switch Name | LED Name |
---|---|---|
SAM E70 Xplained Ultra Evaluation Kit | SW0 | LED1 |
SAM V71 Xplained Ultra Evaluation Kit | SW0 | LED0 |