11.3.2 Memory Access
For read/write operations, the Flash memory can be accessed from either the code space
or the CPU data space. The Flash is accessible through the LPM and
SPM instructions when using the code space.
Additionally, when accessed through the CPU data space, the Flash memory is byte
accessible, meaning that it shares the same address space and access instructions as
SRAM, EEPROM and I/O registers, and it is accessible using
LD/ST instructions.
For the LPM and SPM instructions, address
0x0000 is the start of the Flash, but for LD and
ST, it is 0x8000, as shown in the Memory Map
section.
Addressing Flash Memory in Code Space
For read and write access to the Flash memory in the code space, use the Z-pointer for LPM/SPM access.
The Flash is word-accessed and organized in pages, so the Address Pointer can be treated as having two sections, as shown in the figure above. The word address in the page (FWORD) is held by the Least Significant bits (LSbs) in the Address Pointer, while the Most Significant bits (MSbs) in the Address Pointer hold the Flash page address (FPAGE). Together, FWORD and FPAGE hold an absolute address to a word in the Flash.
The Flash is word-accessed for code space write operations, so the Least Significant bit (bit 0) in the Address Pointer is ignored.
For Flash read operations, one byte is read at a time. The Least
Significant bit (bit 0) in the Address Pointer is used to select the low or high byte in
the word address for this. If this bit is ‘0’, the low byte is read,
and if this bit is ‘1’, the high byte is read.
While initiating a programming operation, the address is latched, and the Address Pointer can be updated and used for other operations.
Addressing Flash in CPU Data Space
The CPU data space is limited to 32 KB. For devices with a Flash memory size greater than 32 KB, the Flash memory is divided into blocks of 32 KB. Those blocks are mapped into data space using the FLMAP bit field of the Control B (CTRLB) register.
For read and write access to the Flash memory in the CPU data space, the
LD/ST instructions are used to access one byte at a
time.