4.5.4 The Special DOT Symbol
The special symbol ‘.’ refers to the current address that is being assembled into. Thus, the expression:
melvin: .word . ; in a data section
defines melvin to contain its own data address. Assigning a value to . is treated the same as a .org directive. Thus the expression:
. = .+2
is the same as saying:
.org .+2
The symbol ‘$’ is accepted as a synonym for ‘.’.
When used in an executable section, ‘.’
refers to a PC address. The PC increments by 4 for each instruction word. In all
architectures, odd values are not permitted.
Note: Instruction words in the PIC32A architecture are 4 bytes long, and may contain 1 or 2 instructions. For
this reason the use of a "dot expression" as a branch target is risky and could result in a
misaligned branch target address. The assembler will issue a strong warning if such usage
is detected.