11.3.3.2 data [DD]

The data attribute specifies that a section should be allocated as initialized storage in data memory, as defined by region data in the linker script. The following attributes may be used in conjunction with data and will further specify the allocation:

  • address() specifies an absolute address
  • near specifies the first 64K of data memory
  • xmemory specifies X address space, which includes all of region data below the address __YDATA_BASE as defined in the linker script
  • ymemory specifies Y address space, which includes all of region data above the address __YDATA_BASE as defined in the linker script
  • align() specifies alignment of the section starting address
  • reverse() specifies alignment of the section ending address + 1