7.3.5 Map File
The map files produced by the linker consist of:
- Archive Member Table
- Lists the name of any members from archive files that are included in the link.
- Memory-Usage Report
- Shows the starting address and length of all output sections in program memory and data memory. It also shows a percent utilization of memory in the region.
- Memory-Usage Report by Module
- Shows the memory usage (text, data, and bss sections) per object file. This report indicates the size in the final ELF file attributable to each input object. A miscellaneous entry also shows those sections whose input object file cannot be determined or the type of memory cannot be established.
- Memory Configuration
- Lists all of the memory regions defined for the link.
- Linker Script and Memory Map
- Shows modules, sections and symbols that are included in the link as specified in the linker script.
- Outside Cross Reference Table (optional)
- Shows symbols, sorted by name. For each symbol, a list of file names is given. If the symbol is defined, the first file listed is the location of the definition. The remaining files listed contain references to the symbol.
A typical map file showing the Memory-Usage Report and the Memory-Usage Report by Module is
presented
below.
Archive member included to satisfy reference by file (symbol)
/Applications/microchip/xc32/v4.30/bin/bin/../../lib/gcc/pic32c/8.3.1/../../../../pic32c/lib/thumb/v7e-m+dp/hard/libpic32c.a(data_init_wrapper.o)
startup_atsamv71j19b.o (__pic32c_data_initialization)
/Applications/microchip/xc32/v4.30/bin/bin/../../lib/gcc/pic32c/8.3.1/../../../../pic32c/lib/thumb/v7e-m+dp/hard/libpic32c.a(data_init_0_1.o)
/Applications/microchip/xc32/v4.30/bin/bin/../../lib/gcc/pic32c/8.3.1/../../../../pic32c/lib/thumb/v7e-m+dp/hard/libpic32c.a(data_init_wrapper.o) (__pic32c_data_initialization_impl)
/Applications/microchip/xc32/v4.30/bin/bin/../../lib/gcc/pic32c/8.3.1/../../../../pic32c/lib/thumb/v7e-m+dp/hard/libc-musl.a(__libc_start_main.o)
startup_atsamv71j19b.o (__libc_init_array)
/Applications/microchip/xc32/v4.30/bin/bin/../../lib/gcc/pic32c/8.3.1/../../../../pic32c/lib/thumb/v7e-m+dp/hard/libc-musl.a(libc.o)
/Applications/microchip/xc32/v4.30/bin/bin/../../lib/gcc/pic32c/8.3.1/../../../../pic32c/lib/thumb/v7e-m+dp/hard/libc-musl.a(__libc_start_main.o) (__progname_full)
/Applications/microchip/xc32/v4.30/bin/bin/../../lib/gcc/pic32c/8.3.1/../../../../pic32c/lib/thumb/v7e-m+dp/hard/libc-musl.a(__environ.o)
/Applications/microchip/xc32/v4.30/bin/bin/../../lib/gcc/pic32c/8.3.1/../../../../pic32c/lib/thumb/v7e-m+dp/hard/libc-musl.a(__libc_start_main.o) (__environ)
Microchip PIC32 Memory-Usage Report
ROM Program-Memory Usage
section address length [bytes] (dec) Description
------- ---------- ------------------------- -----------
.vectors 0x400000 0x168 360
.text 0x400168 0x20 32 App's exec code
.text 0x400188 0x110 272 App's exec code
.text.Reset_Handler 0x400298 0x8c 140
.text.__pic32c_data_ini 0x400324 0x68 104
.text.__libc_start_init 0x40038c 0x5c 92
.dinit 0x4003e8 0x50 80
.text 0x400438 0x40 64 App's exec code
.text.main 0x400478 0x30 48
.text.__pic32c_data_ini 0x4004a8 0x4 4
.text.Dummy_Handler 0x4004ac 0x2 2
.text.__dummy 0x4004ae 0x2 2
Total ROM used : 0x4b0 1200 0.2% of 0x80000
--------------------------------------------------------------------------
Total Program Memory used : 0x4b0 1200 0.2% of 0x80000
--------------------------------------------------------------------------
RAM Data-Memory Usage
section address length [bytes] (dec) Description
------- ---------- ------------------------- -----------
.bss 0x20400000 0x6c 108 Uninitialized data
.bss 0x2040006c 0x4 4 Uninitialized data
.bss 0x20400070 0x14 20 Uninitialized data
.bss 0x20400084 0x4 4 Uninitialized data
Total RAM used : 0x88 136 0.1% of 0x40000
--------------------------------------------------------------------------
Total Data Memory used : 0x88 136 0.1% of 0x40000
--------------------------------------------------------------------------
Dynamic Data-Memory Reservation
section address length [bytes] (dec) Description
------- ---------- ------------------------- -----------
heap 0x20400090 0x10 16 Reserved for heap
stack 0x204000b8 0x3ff40 261952 Reserved for stack
--------------------------------------------------------------------------
Microchip PIC32 Memory-Usage Report By Module
text data bss dec hex basename filename
--------------------------------------------------------------------------------
774 0 0 774 306 startup_atsamv71j19b.ostartup_atsamv71j19b.o
104 0 4 108 6c data_init_0_1.o libpic32c.a
72 0 28 100 64 crtbegin.o /Applications/microchip/xc32/v4.30/bin/bin/../../lib/gcc/pic32c/8.3.1/thumb/v7e-m+dp/hard/crtbegin.o
94 0 0 94 5e __libc_start_main.o libc-musl.a
0 0 80 80 50 libc.o libc-musl.a
80 0 0 80 50 data_init data_init
48 0 20 68 44 xc32_floats.o build/default/production/_ext/1472/xc32_floats.o
16 0 0 16 10 crtn.o /Applications/microchip/xc32/v4.30/bin/bin/../../lib/gcc/pic32c/8.3.1/thumb/v7e-m+dp/hard/crtn.o
8 0 0 8 8 crti.o /Applications/microchip/xc32/v4.30/bin/bin/../../lib/gcc/pic32c/8.3.1/thumb/v7e-m+dp/hard/crti.o
4 0 0 4 4 data_init_wrapper.o libpic32c.a
0 0 4 4 4 __environ.o libc-musl.a
--------------------------------------------------------------------------------
1200 0 136 1336 538 dist/default/production/XC32_sam_library_example.X.production.elf
Discarded input sections
.text 0x00000000 0x0 /Applications/microchip/xc32/v4.30/bin/bin/../../lib/gcc/pic32c/8.3.1/thumb/v7e-m+dp/hard/crti.o
.data 0x00000000 0x0 /Applications/microchip/xc32/v4.30/bin/bin/../../lib/gcc/pic32c/8.3.1/thumb/v7e-m+dp/hard/crti.o
.bss 0x00000000 0x0 /Applications/microchip/xc32/v4.30/bin/bin/../../lib/gcc/pic32c/8.3.1/thumb/v7e-m+dp/hard/crti.o
.xc_stack_usage.hdr
0x00000000 0xe /Applications/microchip/xc32/v4.30/bin/bin/../../lib/gcc/pic32c/8.3.1/thumb/v7e-m+dp/hard/crti.o
.xc_stack_usage
0x00000000 0x26 /Applications/microchip/xc32/v4.30/bin/bin/../../lib/gcc/pic32c/8.3.1/thumb/v7e-m+dp/hard/crti.o
.data 0x00000000 0x4 /Applications/microchip/xc32/v4.30/bin/bin/../../lib/gcc/pic32c/8.3.1/thumb/v7e-m+dp/hard/crtbegin.o
.xc_stack_usage
0x00000000 0x3c /Applications/microchip/xc32/v4.30/bin/bin/../../lib/gcc/pic32c/8.3.1/thumb/v7e-m+dp/hard/crtbegin.o
.xc_stack_usage.hdr
0x00000000 0xe /Applications/microchip/xc32/v4.30/bin/bin/../../lib/gcc/pic32c/8.3.1/thumb/v7e-m+dp/hard/crtbegin.o
.text 0x00000000 0x0 build/default/production/_ext/1472/xc32_floats.o
.data 0x00000000 0x0 build/default/production/_ext/1472/xc32_floats.o
.data 0x00000000 0x0 startup_atsamv71j19b.o
.bss 0x00000000 0x0 startup_atsamv71j19b.o
.text 0x00000000 0x0 /Applications/microchip/xc32/v4.30/bin/bin/../../lib/gcc/pic32c/8.3.1/../../../../pic32c/lib/thumb/v7e-m+dp/hard/libpic32c.a(data_init_wrapper.o)
.data 0x00000000 0x0 /Applications/microchip/xc32/v4.30/bin/bin/../../lib/gcc/pic32c/8.3.1/../../../../pic32c/lib/thumb/v7e-m+dp/hard/libpic32c.a(data_init_wrapper.o)
.bss 0x00000000 0x0 /Applications/microchip/xc32/v4.30/bin/bin/../../lib/gcc/pic32c/8.3.1/../../../../pic32c/lib/thumb/v7e-m+dp/hard/libpic32c.a(data_init_wrapper.o)
.xc_stack_usage
0x00000000 0x2a /Applications/microchip/xc32/v4.30/bin/bin/../../lib/gcc/pic32c/8.3.1/../../../../pic32c/lib/thumb/v7e-m+dp/hard/libpic32c.a(data_init_wrapper.o)
.xc_stack_usage.hdr
0x00000000 0xe /Applications/microchip/xc32/v4.30/bin/bin/../../lib/gcc/pic32c/8.3.1/../../../../pic32c/lib/thumb/v7e-m+dp/hard/libpic32c.a(data_init_wrapper.o)
.text 0x00000000 0x0 /Applications/microchip/xc32/v4.30/bin/bin/../../lib/gcc/pic32c/8.3.1/../../../../pic32c/lib/thumb/v7e-m+dp/hard/libpic32c.a(data_init_0_1.o)
.data 0x00000000 0x0 /Applications/microchip/xc32/v4.30/bin/bin/../../lib/gcc/pic32c/8.3.1/../../../../pic32c/lib/thumb/v7e-m+dp/hard/libpic32c.a(data_init_0_1.o)
.xc_stack_usage
0x00000000 0x2f /Applications/microchip/xc32/v4.30/bin/bin/../../lib/gcc/pic32c/8.3.1/../../../../pic32c/lib/thumb/v7e-m+dp/hard/libpic32c.a(data_init_0_1.o)
.xc_stack_usage.hdr
0x00000000 0xe /Applications/microchip/xc32/v4.30/bin/bin/../../lib/gcc/pic32c/8.3.1/../../../../pic32c/lib/thumb/v7e-m+dp/hard/libpic32c.a(data_init_0_1.o)
.text 0x00000000 0x0 /Applications/microchip/xc32/v4.30/bin/bin/../../lib/gcc/pic32c/8.3.1/../../../../pic32c/lib/thumb/v7e-m+dp/hard/libc-musl.a(__libc_start_main.o)
.data 0x00000000 0x0 /Applications/microchip/xc32/v4.30/bin/bin/../../lib/gcc/pic32c/8.3.1/../../../../pic32c/lib/thumb/v7e-m+dp/hard/libc-musl.a(__libc_start_main.o)
.bss 0x00000000 0x0 /Applications/microchip/xc32/v4.30/bin/bin/../../lib/gcc/pic32c/8.3.1/../../../../pic32c/lib/thumb/v7e-m+dp/hard/libc-musl.a(__libc_start_main.o)
.xc_stack_usage
0x00000000 0x34 /Applications/microchip/xc32/v4.30/bin/bin/../../lib/gcc/pic32c/8.3.1/../../../../pic32c/lib/thumb/v7e-m+dp/hard/libc-musl.a(__libc_start_main.o)
.xc_stack_usage.hdr
0x00000000 0xe /Applications/microchip/xc32/v4.30/bin/bin/../../lib/gcc/pic32c/8.3.1/../../../../pic32c/lib/thumb/v7e-m+dp/hard/libc-musl.a(__libc_start_main.o)
.text 0x00000000 0x0 /Applications/microchip/xc32/v4.30/bin/bin/../../lib/gcc/pic32c/8.3.1/../../../../pic32c/lib/thumb/v7e-m+dp/hard/libc-musl.a(libc.o)
.data 0x00000000 0x0 /Applications/microchip/xc32/v4.30/bin/bin/../../lib/gcc/pic32c/8.3.1/../../../../pic32c/lib/thumb/v7e-m+dp/hard/libc-musl.a(libc.o)
.xc_stack_usage.hdr
0x00000000 0xe /Applications/microchip/xc32/v4.30/bin/bin/../../lib/gcc/pic32c/8.3.1/../../../../pic32c/lib/thumb/v7e-m+dp/hard/libc-musl.a(libc.o)
.text 0x00000000 0x0 /Applications/microchip/xc32/v4.30/bin/bin/../../lib/gcc/pic32c/8.3.1/../../../../pic32c/lib/thumb/v7e-m+dp/hard/libc-musl.a(__environ.o)
.data 0x00000000 0x0 /Applications/microchip/xc32/v4.30/bin/bin/../../lib/gcc/pic32c/8.3.1/../../../../pic32c/lib/thumb/v7e-m+dp/hard/libc-musl.a(__environ.o)
.xc_stack_usage.hdr
0x00000000 0xe /Applications/microchip/xc32/v4.30/bin/bin/../../lib/gcc/pic32c/8.3.1/../../../../pic32c/lib/thumb/v7e-m+dp/hard/libc-musl.a(__environ.o)
.text 0x00000000 0x0 /Applications/microchip/xc32/v4.30/bin/bin/../../lib/gcc/pic32c/8.3.1/thumb/v7e-m+dp/hard/crtend.o
.data 0x00000000 0x0 /Applications/microchip/xc32/v4.30/bin/bin/../../lib/gcc/pic32c/8.3.1/thumb/v7e-m+dp/hard/crtend.o
.bss 0x00000000 0x0 /Applications/microchip/xc32/v4.30/bin/bin/../../lib/gcc/pic32c/8.3.1/thumb/v7e-m+dp/hard/crtend.o
.eh_frame 0x00000000 0x4 /Applications/microchip/xc32/v4.30/bin/bin/../../lib/gcc/pic32c/8.3.1/thumb/v7e-m+dp/hard/crtend.o
.xc_stack_usage.hdr
0x00000000 0xe /Applications/microchip/xc32/v4.30/bin/bin/../../lib/gcc/pic32c/8.3.1/thumb/v7e-m+dp/hard/crtend.o
.comment 0x00000000 0x30 /Applications/microchip/xc32/v4.30/bin/bin/../../lib/gcc/pic32c/8.3.1/thumb/v7e-m+dp/hard/crtend.o
.ARM.attributes
0x00000000 0x30 /Applications/microchip/xc32/v4.30/bin/bin/../../lib/gcc/pic32c/8.3.1/thumb/v7e-m+dp/hard/crtend.o
.text 0x00000000 0x0 /Applications/microchip/xc32/v4.30/bin/bin/../../lib/gcc/pic32c/8.3.1/thumb/v7e-m+dp/hard/crtn.o
.data 0x00000000 0x0 /Applications/microchip/xc32/v4.30/bin/bin/../../lib/gcc/pic32c/8.3.1/thumb/v7e-m+dp/hard/crtn.o
.bss 0x00000000 0x0 /Applications/microchip/xc32/v4.30/bin/bin/../../lib/gcc/pic32c/8.3.1/thumb/v7e-m+dp/hard/crtn.o
.xc_stack_usage.hdr
0x00000000 0xe /Applications/microchip/xc32/v4.30/bin/bin/../../lib/gcc/pic32c/8.3.1/thumb/v7e-m+dp/hard/crtn.o
Memory Configuration
Name Origin Length Attributes
rom 0x00400000 0x00080000 xrl
ram 0x20400000 0x00040000 xw !r
itcm 0x00000000 0x00000000 xw
dtcm 0x20000000 0x00000000 xw !r
*default* 0x00000000 0xffffffff
Linker script and memory map
LOAD /Applications/microchip/xc32/v4.30/bin/bin/../../lib/gcc/pic32c/8.3.1/thumb/v7e-m+dp/hard/crti.o
LOAD /Applications/microchip/xc32/v4.30/bin/bin/../../lib/gcc/pic32c/8.3.1/thumb/v7e-m+dp/hard/crtbegin.o
LOAD build/default/production/_ext/1472/xc32_floats.o
0x00000001 __MPLAB_BUILD = 0x1
LOAD startup_atsamv71j19b.o
START GROUP
LOAD /Applications/microchip/xc32/v4.30/bin/bin/../../lib/gcc/pic32c/8.3.1/../../../../pic32c/lib/thumb/v7e-m+dp/hard/libpic32c.a
LOAD /Applications/microchip/xc32/v4.30/bin/bin/../../lib/gcc/pic32c/8.3.1/../../../../pic32c/lib/thumb/v7e-m+dp/hard/libm-emfloat.a
LOAD /Applications/microchip/xc32/v4.30/bin/bin/../../lib/gcc/pic32c/8.3.1/../../../../pic32c/lib/thumb/v7e-m+dp/hard/libc-musl.a
LOAD /Applications/microchip/xc32/v4.30/bin/bin/../../lib/gcc/pic32c/8.3.1/../../../../pic32c/lib/thumb/v7e-m+dp/hard/libm-emfloat.a
LOAD /Applications/microchip/xc32/v4.30/bin/bin/../../lib/gcc/pic32c/8.3.1/thumb/v7e-m+dp/hard/libgcc.a
END GROUP
LOAD /Applications/microchip/xc32/v4.30/bin/bin/../../lib/gcc/pic32c/8.3.1/thumb/v7e-m+dp/hard/crtend.o
LOAD /Applications/microchip/xc32/v4.30/bin/bin/../../lib/gcc/pic32c/8.3.1/thumb/v7e-m+dp/hard/crtn.o
0x00480000 __rom_end = (ORIGIN (rom) + LENGTH (rom))
0x20440000 __ram_end = (ORIGIN (ram) + LENGTH (ram))
.vectors 0x00400000 0x168
0x00400000 . = ALIGN (0x4)
0x00400000 _sfixed = .
*(.vectors .vectors.* .vectors_default .vectors_default.*)
.vectors.default
0x00400000 0x168 startup_atsamv71j19b.o
0x00400000 exception_table
*(.isr_vector)
*(.reset*)
*(.after_vectors)
.text 0x00400168 0x20
0x00400168 . = ALIGN (0x4)
*(.glue_7t)
.glue_7t 0x00400168 0x0 linker stubs
*(.glue_7)
.glue_7 0x00400168 0x0 linker stubs
*(.gnu.linkonce.r.*)
*(.ARM.extab* .gnu.linkonce.armextab.*)
0x00400168 . = ALIGN (0x4)
*(.init)
.init 0x00400168 0x4 /Applications/microchip/xc32/v4.30/bin/bin/../../lib/gcc/pic32c/8.3.1/thumb/v7e-m+dp/hard/crti.o
0x00400168 _init
.init 0x0040016c 0x8 /Applications/microchip/xc32/v4.30/bin/bin/../../lib/gcc/pic32c/8.3.1/thumb/v7e-m+dp/hard/crtn.o
0x00400174 . = ALIGN (0x4)
0x00400174 __preinit_array_start = .
*(.preinit_array)
0x00400174 __preinit_array_end = .
0x00400174 . = ALIGN (0x4)
0x00400174 __init_array_start = .
*(SORT_BY_NAME(.init_array.*))
*(.init_array)
.init_array 0x00400174 0x4 /Applications/microchip/xc32/v4.30/bin/bin/../../lib/gcc/pic32c/8.3.1/thumb/v7e-m+dp/hard/crtbegin.o
0x00400178 __init_array_end = .
0x00400178 . = ALIGN (0x4)
*crtbegin.o(.ctors)
*(EXCLUDE_FILE(*crtend.o) .ctors)
*(SORT_BY_NAME(.ctors.*))
*crtend.o(.ctors)
0x00400178 . = ALIGN (0x4)
*(.fini)
.fini 0x00400178 0x4 /Applications/microchip/xc32/v4.30/bin/bin/../../lib/gcc/pic32c/8.3.1/thumb/v7e-m+dp/hard/crti.o
0x00400178 _fini
.fini 0x0040017c 0x8 /Applications/microchip/xc32/v4.30/bin/bin/../../lib/gcc/pic32c/8.3.1/thumb/v7e-m+dp/hard/crtn.o
0x00400184 . = ALIGN (0x4)
0x00400184 __fini_array_start = .
*(.fini_array)
.fini_array 0x00400184 0x4 /Applications/microchip/xc32/v4.30/bin/bin/../../lib/gcc/pic32c/8.3.1/thumb/v7e-m+dp/hard/crtbegin.o
*(SORT_BY_NAME(.fini_array.*))
0x00400188 __fini_array_end = .
*crtbegin.o(.dtors)
*(EXCLUDE_FILE(*crtend.o) .dtors)
*(SORT_BY_NAME(.dtors.*))
*crtend.o(.dtors)
0x00400188 . = ALIGN (0x4)
0x00400188 _efixed = .
[!provide] PROVIDE (__exidx_start = .)
.ARM.exidx
*(.ARM.exidx* .gnu.linkonce.armexidx.*)
[!provide] PROVIDE (__exidx_end = .)
0x00400188 . = ALIGN (0x4)
0x00400188 _etext = .
.bss 0x20400000 0x0
0x20400000 . = ALIGN (0x4)
0x20400000 __bss_start__ = .
0x20400000 _sbss = .
0x20400000 _szero = .
*(COMMON)
0x20400000 . = ALIGN (0x4)
0x20400000 __bss_end__ = .
0x20400000 _ebss = .
0x20400000 _ezero = .
0x20400000 . = ALIGN (0x4)
0x20400000 _end = .
0x2043ffff _ram_end_ = ((ORIGIN (ram) + LENGTH (ram)) - 0x1)
OUTPUT(dist/default/production/XC32_sam_library_example.X.production.elf elf32-littlearm)
LOAD stack
LOAD data_init
.ARM.attributes
0x00000000 0x32
.ARM.attributes
0x00000000 0x1e /Applications/microchip/xc32/v4.30/bin/bin/../../lib/gcc/pic32c/8.3.1/thumb/v7e-m+dp/hard/crti.o
.ARM.attributes
0x0000001e 0x32 /Applications/microchip/xc32/v4.30/bin/bin/../../lib/gcc/pic32c/8.3.1/thumb/v7e-m+dp/hard/crtbegin.o
.ARM.attributes
0x00000050 0x32 build/default/production/_ext/1472/xc32_floats.o
.ARM.attributes
0x00000082 0x32 startup_atsamv71j19b.o
.ARM.attributes
0x000000b4 0x32 /Applications/microchip/xc32/v4.30/bin/bin/../../lib/gcc/pic32c/8.3.1/../../../../pic32c/lib/thumb/v7e-m+dp/hard/libpic32c.a(data_init_wrapper.o)
.ARM.attributes
0x000000e6 0x32 /Applications/microchip/xc32/v4.30/bin/bin/../../lib/gcc/pic32c/8.3.1/../../../../pic32c/lib/thumb/v7e-m+dp/hard/libpic32c.a(data_init_0_1.o)
.ARM.attributes
0x00000118 0x34 /Applications/microchip/xc32/v4.30/bin/bin/../../lib/gcc/pic32c/8.3.1/../../../../pic32c/lib/thumb/v7e-m+dp/hard/libc-musl.a(__libc_start_main.o)
.ARM.attributes
0x0000014c 0x32 /Applications/microchip/xc32/v4.30/bin/bin/../../lib/gcc/pic32c/8.3.1/../../../../pic32c/lib/thumb/v7e-m+dp/hard/libc-musl.a(libc.o)
.ARM.attributes
0x0000017e 0x32 /Applications/microchip/xc32/v4.30/bin/bin/../../lib/gcc/pic32c/8.3.1/../../../../pic32c/lib/thumb/v7e-m+dp/hard/libc-musl.a(__environ.o)
.ARM.attributes
0x000001b0 0x1e /Applications/microchip/xc32/v4.30/bin/bin/../../lib/gcc/pic32c/8.3.1/thumb/v7e-m+dp/hard/crtn.o
.comment 0x00000000 0x2f
.comment 0x00000000 0x2f /Applications/microchip/xc32/v4.30/bin/bin/../../lib/gcc/pic32c/8.3.1/thumb/v7e-m+dp/hard/crtbegin.o
0x30 (size before relaxing)
.comment 0x0000002f 0x30 build/default/production/_ext/1472/xc32_floats.o
.comment 0x0000002f 0x30 startup_atsamv71j19b.o
.comment 0x0000002f 0x30 /Applications/microchip/xc32/v4.30/bin/bin/../../lib/gcc/pic32c/8.3.1/../../../../pic32c/lib/thumb/v7e-m+dp/hard/libpic32c.a(data_init_wrapper.o)
.comment 0x0000002f 0x30 /Applications/microchip/xc32/v4.30/bin/bin/../../lib/gcc/pic32c/8.3.1/../../../../pic32c/lib/thumb/v7e-m+dp/hard/libpic32c.a(data_init_0_1.o)
.comment 0x0000002f 0x30 /Applications/microchip/xc32/v4.30/bin/bin/../../lib/gcc/pic32c/8.3.1/../../../../pic32c/lib/thumb/v7e-m+dp/hard/libc-musl.a(__libc_start_main.o)
.comment 0x0000002f 0x30 /Applications/microchip/xc32/v4.30/bin/bin/../../lib/gcc/pic32c/8.3.1/../../../../pic32c/lib/thumb/v7e-m+dp/hard/libc-musl.a(libc.o)
.comment 0x0000002f 0x30 /Applications/microchip/xc32/v4.30/bin/bin/../../lib/gcc/pic32c/8.3.1/../../../../pic32c/lib/thumb/v7e-m+dp/hard/libc-musl.a(__environ.o)
.debug_info 0x00000000 0x1666
.debug_info 0x00000000 0x318 build/default/production/_ext/1472/xc32_floats.o
.debug_info 0x00000318 0x2a2 /Applications/microchip/xc32/v4.30/bin/bin/../../lib/gcc/pic32c/8.3.1/../../../../pic32c/lib/thumb/v7e-m+dp/hard/libpic32c.a(data_init_wrapper.o)
.debug_info 0x000005ba 0x2a5 /Applications/microchip/xc32/v4.30/bin/bin/../../lib/gcc/pic32c/8.3.1/../../../../pic32c/lib/thumb/v7e-m+dp/hard/libpic32c.a(data_init_0_1.o)
.debug_info 0x0000085f 0x623 /Applications/microchip/xc32/v4.30/bin/bin/../../lib/gcc/pic32c/8.3.1/../../../../pic32c/lib/thumb/v7e-m+dp/hard/libc-musl.a(__libc_start_main.o)
.debug_info 0x00000e82 0x535 /Applications/microchip/xc32/v4.30/bin/bin/../../lib/gcc/pic32c/8.3.1/../../../../pic32c/lib/thumb/v7e-m+dp/hard/libc-musl.a(libc.o)
.debug_info 0x000013b7 0x2af /Applications/microchip/xc32/v4.30/bin/bin/../../lib/gcc/pic32c/8.3.1/../../../../pic32c/lib/thumb/v7e-m+dp/hard/libc-musl.a(__environ.o)
.debug_abbrev 0x00000000 0x2d6
.debug_abbrev 0x00000000 0x57 build/default/production/_ext/1472/xc32_floats.o
.debug_abbrev 0x00000057 0x2b /Applications/microchip/xc32/v4.30/bin/bin/../../lib/gcc/pic32c/8.3.1/../../../../pic32c/lib/thumb/v7e-m+dp/hard/libpic32c.a(data_init_wrapper.o)
.debug_abbrev 0x00000082 0x2e /Applications/microchip/xc32/v4.30/bin/bin/../../lib/gcc/pic32c/8.3.1/../../../../pic32c/lib/thumb/v7e-m+dp/hard/libpic32c.a(data_init_0_1.o)
.debug_abbrev 0x000000b0 0x117 /Applications/microchip/xc32/v4.30/bin/bin/../../lib/gcc/pic32c/8.3.1/../../../../pic32c/lib/thumb/v7e-m+dp/hard/libc-musl.a(__libc_start_main.o)
.debug_abbrev 0x000001c7 0xb8 /Applications/microchip/xc32/v4.30/bin/bin/../../lib/gcc/pic32c/8.3.1/../../../../pic32c/lib/thumb/v7e-m+dp/hard/libc-musl.a(libc.o)
.debug_abbrev 0x0000027f 0x57 /Applications/microchip/xc32/v4.30/bin/bin/../../lib/gcc/pic32c/8.3.1/../../../../pic32c/lib/thumb/v7e-m+dp/hard/libc-musl.a(__environ.o)
.debug_aranges 0x00000000 0xb8
.debug_aranges
0x00000000 0x20 build/default/production/_ext/1472/xc32_floats.o
.debug_aranges
0x00000020 0x20 /Applications/microchip/xc32/v4.30/bin/bin/../../lib/gcc/pic32c/8.3.1/../../../../pic32c/lib/thumb/v7e-m+dp/hard/libpic32c.a(data_init_wrapper.o)
.debug_aranges
0x00000040 0x20 /Applications/microchip/xc32/v4.30/bin/bin/../../lib/gcc/pic32c/8.3.1/../../../../pic32c/lib/thumb/v7e-m+dp/hard/libpic32c.a(data_init_0_1.o)
.debug_aranges
0x00000060 0x28 /Applications/microchip/xc32/v4.30/bin/bin/../../lib/gcc/pic32c/8.3.1/../../../../pic32c/lib/thumb/v7e-m+dp/hard/libc-musl.a(__libc_start_main.o)
.debug_aranges
0x00000088 0x18 /Applications/microchip/xc32/v4.30/bin/bin/../../lib/gcc/pic32c/8.3.1/../../../../pic32c/lib/thumb/v7e-m+dp/hard/libc-musl.a(libc.o)
.debug_aranges
0x000000a0 0x18 /Applications/microchip/xc32/v4.30/bin/bin/../../lib/gcc/pic32c/8.3.1/../../../../pic32c/lib/thumb/v7e-m+dp/hard/libc-musl.a(__environ.o)
.debug_ranges 0x00000000 0x70
.debug_ranges 0x00000000 0x10 build/default/production/_ext/1472/xc32_floats.o
.debug_ranges 0x00000010 0x10 /Applications/microchip/xc32/v4.30/bin/bin/../../lib/gcc/pic32c/8.3.1/../../../../pic32c/lib/thumb/v7e-m+dp/hard/libpic32c.a(data_init_wrapper.o)
.debug_ranges 0x00000020 0x10 /Applications/microchip/xc32/v4.30/bin/bin/../../lib/gcc/pic32c/8.3.1/../../../../pic32c/lib/thumb/v7e-m+dp/hard/libpic32c.a(data_init_0_1.o)
.debug_ranges 0x00000030 0x40 /Applications/microchip/xc32/v4.30/bin/bin/../../lib/gcc/pic32c/8.3.1/../../../../pic32c/lib/thumb/v7e-m+dp/hard/libc-musl.a(__libc_start_main.o)
.debug_line 0x00000000 0x5ab
.debug_line 0x00000000 0x73 build/default/production/_ext/1472/xc32_floats.o
.debug_line 0x00000073 0xa7 /Applications/microchip/xc32/v4.30/bin/bin/../../lib/gcc/pic32c/8.3.1/../../../../pic32c/lib/thumb/v7e-m+dp/hard/libpic32c.a(data_init_wrapper.o)
.debug_line 0x0000011a 0x101 /Applications/microchip/xc32/v4.30/bin/bin/../../lib/gcc/pic32c/8.3.1/../../../../pic32c/lib/thumb/v7e-m+dp/hard/libpic32c.a(data_init_0_1.o)
.debug_line 0x0000021b 0x1d1 /Applications/microchip/xc32/v4.30/bin/bin/../../lib/gcc/pic32c/8.3.1/../../../../pic32c/lib/thumb/v7e-m+dp/hard/libc-musl.a(__libc_start_main.o)
.debug_line 0x000003ec 0xba /Applications/microchip/xc32/v4.30/bin/bin/../../lib/gcc/pic32c/8.3.1/../../../../pic32c/lib/thumb/v7e-m+dp/hard/libc-musl.a(libc.o)
.debug_line 0x000004a6 0x105 /Applications/microchip/xc32/v4.30/bin/bin/../../lib/gcc/pic32c/8.3.1/../../../../pic32c/lib/thumb/v7e-m+dp/hard/libc-musl.a(__environ.o)
.debug_str 0x00000000 0x0
.debug_str 0x00000000 0x0 build/default/production/_ext/1472/xc32_floats.o
.debug_str 0x00000000 0x0 /Applications/microchip/xc32/v4.30/bin/bin/../../lib/gcc/pic32c/8.3.1/../../../../pic32c/lib/thumb/v7e-m+dp/hard/libpic32c.a(data_init_wrapper.o)
.debug_str 0x00000000 0x0 /Applications/microchip/xc32/v4.30/bin/bin/../../lib/gcc/pic32c/8.3.1/../../../../pic32c/lib/thumb/v7e-m+dp/hard/libpic32c.a(data_init_0_1.o)
.debug_str 0x00000000 0x0 /Applications/microchip/xc32/v4.30/bin/bin/../../lib/gcc/pic32c/8.3.1/../../../../pic32c/lib/thumb/v7e-m+dp/hard/libc-musl.a(__libc_start_main.o)
.debug_str 0x00000000 0x0 /Applications/microchip/xc32/v4.30/bin/bin/../../lib/gcc/pic32c/8.3.1/../../../../pic32c/lib/thumb/v7e-m+dp/hard/libc-musl.a(libc.o)
.debug_str 0x00000000 0x0 /Applications/microchip/xc32/v4.30/bin/bin/../../lib/gcc/pic32c/8.3.1/../../../../pic32c/lib/thumb/v7e-m+dp/hard/libc-musl.a(__environ.o)
.debug_frame 0x00000000 0xa8
.debug_frame 0x00000000 0x20 build/default/production/_ext/1472/xc32_floats.o
.debug_frame 0x00000020 0x20 /Applications/microchip/xc32/v4.30/bin/bin/../../lib/gcc/pic32c/8.3.1/../../../../pic32c/lib/thumb/v7e-m+dp/hard/libpic32c.a(data_init_wrapper.o)
.debug_frame 0x00000040 0x2c /Applications/microchip/xc32/v4.30/bin/bin/../../lib/gcc/pic32c/8.3.1/../../../../pic32c/lib/thumb/v7e-m+dp/hard/libpic32c.a(data_init_0_1.o)
.debug_frame 0x0000006c 0x3c /Applications/microchip/xc32/v4.30/bin/bin/../../lib/gcc/pic32c/8.3.1/../../../../pic32c/lib/thumb/v7e-m+dp/hard/libc-musl.a(__libc_start_main.o)
.debug_loc 0x00000000 0x65
.debug_loc 0x00000000 0x14 /Applications/microchip/xc32/v4.30/bin/bin/../../lib/gcc/pic32c/8.3.1/../../../../pic32c/lib/thumb/v7e-m+dp/hard/libpic32c.a(data_init_0_1.o)
.debug_loc 0x00000014 0x51 /Applications/microchip/xc32/v4.30/bin/bin/../../lib/gcc/pic32c/8.3.1/../../../../pic32c/lib/thumb/v7e-m+dp/hard/libc-musl.a(__libc_start_main.o)
.note.GNU-stack
0x00000000 0x0
.note.GNU-stack
0x00000000 0x0 /Applications/microchip/xc32/v4.30/bin/bin/../../lib/gcc/pic32c/8.3.1/../../../../pic32c/lib/thumb/v7e-m+dp/hard/libc-musl.a(__libc_start_main.o)
.note.GNU-stack
0x00000000 0x0 /Applications/microchip/xc32/v4.30/bin/bin/../../lib/gcc/pic32c/8.3.1/../../../../pic32c/lib/thumb/v7e-m+dp/hard/libc-musl.a(libc.o)
.note.GNU-stack
0x00000000 0x0 /Applications/microchip/xc32/v4.30/bin/bin/../../lib/gcc/pic32c/8.3.1/../../../../pic32c/lib/thumb/v7e-m+dp/hard/libc-musl.a(__environ.o)
.stack 0x204000b8 0x100
.stack 0x204000b8 0x100 stack
.bss%1 0x20400000 0x6c
.bss 0x20400000 0x50 /Applications/microchip/xc32/v4.30/bin/bin/../../lib/gcc/pic32c/8.3.1/../../../../pic32c/lib/thumb/v7e-m+dp/hard/libc-musl.a(libc.o)
0x20400000 program_invocation_name
0x20400000 __progname_full
0x20400004 __progname
0x20400004 program_invocation_short_name
0x20400008 __sysinfo
0x2040000c __hwcap
0x20400010 __libc
.bss 0x20400050 0x1c /Applications/microchip/xc32/v4.30/bin/bin/../../lib/gcc/pic32c/8.3.1/thumb/v7e-m+dp/hard/crtbegin.o
.bss%3 0x20400070 0x14
.bss 0x20400070 0x14 build/default/production/_ext/1472/xc32_floats.o
0x20400070 result
0x20400078 myDouble
0x20400080 myFloat
.bss%4 0x2040006c 0x4
.bss 0x2040006c 0x4 /Applications/microchip/xc32/v4.30/bin/bin/../../lib/gcc/pic32c/8.3.1/../../../../pic32c/lib/thumb/v7e-m+dp/hard/libpic32c.a(data_init_0_1.o)
.bss%5 0x20400084 0x4
.bss 0x20400084 0x4 /Applications/microchip/xc32/v4.30/bin/bin/../../lib/gcc/pic32c/8.3.1/../../../../pic32c/lib/thumb/v7e-m+dp/hard/libc-musl.a(__environ.o)
0x20400084 _environ
0x20400084 __environ
0x20400084 environ
0x20400084 ___environ
.eh_frame%z1 0x00000000 0x0
.eh_frame 0x00000000 0x0 /Applications/microchip/xc32/v4.30/bin/bin/../../lib/gcc/pic32c/8.3.1/thumb/v7e-m+dp/hard/crtbegin.o
.text%6 0x00400188 0x110
.text 0x00400188 0x110 startup_atsamv71j19b.o
.text.Reset_Handler%7
0x00400298 0x8c
.text.Reset_Handler
0x00400298 0x8c startup_atsamv71j19b.o
0x00400298 Reset_Handler
.text.__pic32c_data_initialization_impl%8
0x00400324 0x68
.text.__pic32c_data_initialization_impl
0x00400324 0x68 /Applications/microchip/xc32/v4.30/bin/bin/../../lib/gcc/pic32c/8.3.1/../../../../pic32c/lib/thumb/v7e-m+dp/hard/libpic32c.a(data_init_0_1.o)
0x00400324 __pic32c_data_initialization_impl
0x00400324 __copy_needed
.text.__libc_start_init%9
0x0040038c 0x5c
.text.__libc_start_init
0x0040038c 0x5c /Applications/microchip/xc32/v4.30/bin/bin/../../lib/gcc/pic32c/8.3.1/../../../../pic32c/lib/thumb/v7e-m+dp/hard/libc-musl.a(__libc_start_main.o)
0x0040038c __libc_init_array
.dinit%10 0x004003e8 0x50
.dinit 0x004003e8 0x50 data_init
.text%11 0x00400438 0x40
.text 0x00400438 0x40 /Applications/microchip/xc32/v4.30/bin/bin/../../lib/gcc/pic32c/8.3.1/thumb/v7e-m+dp/hard/crtbegin.o
.text.main%12 0x00400478 0x30
.text.main 0x00400478 0x30 build/default/production/_ext/1472/xc32_floats.o
0x00400478 main
.text.__pic32c_data_initialization%13
0x004004a8 0x4
.text.__pic32c_data_initialization
0x004004a8 0x4 /Applications/microchip/xc32/v4.30/bin/bin/../../lib/gcc/pic32c/8.3.1/../../../../pic32c/lib/thumb/v7e-m+dp/hard/libpic32c.a(data_init_wrapper.o)
0x004004a8 __pic32c_data_initialization
.text.Dummy_Handler%14
0x004004ac 0x2
.text.Dummy_Handler
0x004004ac 0x2 startup_atsamv71j19b.o
0x004004ac TWIHS0_Handler
0x004004ac SVCall_Handler
0x004004ac Reserved18_Handler
0x004004ac TC0_CH2_Handler
0x004004ac Reserved69_Handler
0x004004ac TC3_CH1_Handler
0x004004ac Reserved38_Handler
0x004004ac UART2_Handler
0x004004ac TRNG_Handler
0x004004ac HardFault_Handler
0x004004ac TC2_Handler
0x004004ac Reserved12_Handler
0x004004ac SysTick_Handler
0x004004ac AFEC1_Handler
0x004004ac PendSV_Handler
0x004004ac TC0_CH1_Handler
0x004004ac TC7_Handler
0x004004ac Reserved9_Handler
0x004004ac QSPI_Handler
0x004004ac NonMaskableInt_Handler
0x004004ac ISI_Handler
0x004004ac MCAN0_INT0_Handler
0x004004ac Reserved41_Handler
0x004004ac TC9_Handler
0x004004ac RSWDT_Handler
0x004004ac USART0_Handler
0x004004ac TC1_CH2_Handler
0x004004ac RTT_Handler
0x004004ac USBHS_Handler
0x004004ac IXC_Handler
0x004004ac CCF_Handler
0x004004ac Reserved55_Handler
0x004004ac PIOB_Handler
0x004004ac RTC_Handler
0x004004ac UsageFault_Handler
0x004004ac TC6_Handler
0x004004ac Reserved37_Handler
0x004004ac WDT_Handler
0x004004ac TC4_Handler
0x004004ac TC1_Handler
0x004004ac UART1_Handler
0x004004ac TC3_Handler
0x004004ac Dummy_Handler
0x004004ac TWIHS1_Handler
0x004004ac TC3_CH2_Handler
0x004004ac XDMAC_Handler
0x004004ac TC2_CH0_Handler
0x004004ac PWM1_Handler
0x004004ac USART1_Handler
0x004004ac PWM0_Handler
0x004004ac PIOA_Handler
0x004004ac AFEC0_Handler
0x004004ac CCW_Handler
0x004004ac TC3_CH0_Handler
0x004004ac SSC_Handler
0x004004ac TC11_Handler
0x004004ac TC1_CH0_Handler
0x004004ac Reserved21_Handler
0x004004ac Reserved17_Handler
0x004004ac ACC_Handler
0x004004ac PMC_Handler
0x004004ac GMAC_Handler
0x004004ac TC2_CH2_Handler
0x004004ac Reserved42_Handler
0x004004ac MCAN0_INT1_Handler
0x004004ac GMAC_Q5_Handler
0x004004ac SUPC_Handler
0x004004ac TC2_CH1_Handler
0x004004ac TC8_Handler
0x004004ac EFC_Handler
0x004004ac GMAC_Q1_Handler
0x004004ac GMAC_Q2_Handler
0x004004ac TC1_CH1_Handler
0x004004ac TC10_Handler
0x004004ac GMAC_Q3_Handler
0x004004ac PIOD_Handler
0x004004ac MLB_Handler
0x004004ac Reserved46_Handler
0x004004ac Reserved70_Handler
0x004004ac Reserved62_Handler
0x004004ac UART0_Handler
0x004004ac TC0_CH0_Handler
0x004004ac Reserved45_Handler
0x004004ac Reserved15_Handler
0x004004ac GMAC_Q4_Handler
0x004004ac FPU_Handler
0x004004ac BusFault_Handler
0x004004ac RSTC_Handler
0x004004ac TC0_Handler
0x004004ac MemoryManagement_Handler
0x004004ac Reserved54_Handler
0x004004ac DebugMonitor_Handler
0x004004ac TC5_Handler
0x004004ac ICM_Handler
0x004004ac AES_Handler
0x004004ac DACC_Handler
.text.__dummy%15
0x004004ae 0x2
.text.__dummy 0x004004ae 0x2 /Applications/microchip/xc32/v4.30/bin/bin/../../lib/gcc/pic32c/8.3.1/../../../../pic32c/lib/thumb/v7e-m+dp/hard/libc-musl.a(__libc_start_main.o)
0x004004ae __init_host
0x004004ae __init_stdio