1.30 SQI Flash Read Write

This example application demonstrates how to use the SQI Peripheral library to perform erase, write and read operation with the on-board SST26 SQI Serial Flash memory.

Description

This example uses the SQI peripheral library to erase and write an array of values to the on-board SST26 SQI Serial Flash memory. It verifies the value written by reading the values back and comparing it to the value written.

Downloading and Building the Application

To clone or download this application from Github, go to the main page of this repository and then click Clone button to clone this repository or download as zip file. This content can also be downloaded using content manager by following these instructions.

Path of the application within the repository is apps/sqi/sqi_read_write/firmware.

To build the application, refer to the following table and open the project using its IDE.

Project Name Description
pic32ck_gc01_cult.X MPLABX Project for PIC32CK GC01 Curiosity Ultra board

Setting Up the Hardware

The following table shows the target hardware for the application projects.

Project Name Board
pic32ck_gc01_cult.X PIC32CK GC01 Curiosity Ultra board

Setting Up PIC32CK GC01 Curiosity Ultra Board

  • Connect the Debug USB port on the board to the computer using a micro USB cable

Running the Application

  1. Build and program the application using the its IDE
  2. Press the Switch to start the SQI Transfer
  3. LED is turned ON when the value read from the SQI Serial Flash memory matches with the written value
The following table provides the switch and LED names:
Board Switch Name LED Name
PIC32CK GC01 Curiosity Ultra board SW0 LED0