Introduction
This driver for Atmel® | SMART ARM®-based microcontrollers provides an interface for the configuration and management of the device's Analog Comparator Interface Controller functionality.
The Analog Comparator Interface controls eight Analog Comparators (AC) with identical behavior. Each Analog Comparator compares two voltages, yielding an output that depends on the result of the comparison.
Devices from the following series can use this module:
Atmel | SMART SAM4L
The outline of this documentation is as follows: