1.4.2 PFM Back-to-Back Writes
When repetitive writes to nonvolatile memory (Program Flash Memory) are performed, they could result in write/erase failures at some locations. The issue is due to latent timing in the nonvolatile memory controller, which can cause the write instruction to fail under certain conditions.
Work around
To avoid the issue, it is recommended to wait an additional 100 μs after the NVMCON1.WR bit has been set, allowing for the last word to be loaded into the write buffer.
NVMCON2 = 0x55;
NVMCON2 = 0xAA;
NVMCON1bits.WR = 1;
__delay_us(100);
NVMCON1bits.WREN = 0;
Note: The
__delay_us() function uses a
#define macro definition. For the intrinsic
__delay_us() function to work correctly, the value of the
_XTAL_FREQ must be clearly defined. This macro is defined in the
device_config.h file if the code is generated using MCC. The
value of XTAL_FREQ is equal to the system clock frequency.Affected Silicon Revisions
| A2 | A3 | ||||||
| X | X |