2.1 Issue Summary
When migrating a CLB (Configurable Logic Block) project from a previous version to the latest version (CLB v2.0.0 or later), users encounter the following:
- CLB features are now loaded with the CLB synthesizer library in MCC Melody, so the CLB module may not appear under the Device Resources Driver section as before.
- Previous MCC Melody CLB project configurations may not work as expected due to changes in how CLB is integrated and managed in newer versions.
This is a direct result of architectural changes in MCC Melody and the CLB Synthesizer tool, which now tightly couples CLB configuration with the synthesizer library and content manager.