1.18 SERCOM SPI EEPROM Read Write
This example application demonstrates how to use the SERCOM SPI peripheral to write and read from the SPI serial EEPROM memory.
Description
This example uses the SERCOM SPI peripheral library to write an array of values to the SPI Serial EEPROM and verify the value written by reading the values back and comparing it to the value written.
Downloading and Building the Application
To clone or download this application from Github, go to the main page of this repository and then click Clone button to clone this repository or download as zip file. This content can also be downloaded using content manager by following these instructions.
Path of the application within the repository is apps/sercom/spi/spi_eeprom_write_read/firmware.
To build the application, refer to the following table and open the project using its IDE.
| Project Name | Description | 
|---|---|
| WBZ351_curiosity.X | MPLABX project for PIC32CX WBZ351 Curiosity Board | 
Setting Up the Hardware
The following table shows the target hardware for the application projects.
| Project Name | Board | 
|---|---|
| WBZ351_curiosity.X | PIC32CX WBZ351 Curiosity Board | 
Setting Up PIC32CX WBZ351 Curiosity Board
- Plug an EEPROM 4 Click board into the mikroBUS socket of the PIC32CX WBZ351 Curiosity Board
 - Connect the Debug USB port on the board to the computer using micro USB cable
 
Running the Application
- Build and Program the application project using its IDE
 - LED indicates the success or failure:
- LED is turned ON when the value read from the EEPROM matched with the written value
 - LED is turned OFF when the value read from the EEPROM did not match with
                            the written valueRefer below table for LED name:
Board LED Name PIC32CX WBZ351 Curiosity Board Green LED