2.5 Pin Descriptions

This section contains descriptions of the various LAN8670/1/2 pins. The “_N” symbol in the signal name indicates that the active, or asserted, state occurs when the signal is at a low voltage level. For example, RESET_N indicates that the reset signal is active low. When “_N” is not present after the signal name, the signal is asserted when at the high voltage level.

The terms assertion and negation are used exclusively. This is done to avoid confusion when working with a mixture of “active low” and “active high” signals. The term assert, or assertion, indicates that a signal is active, independent of whether that level is represented by a high or low voltage. The term negate, or negation, indicates that a signal is inactive.

Pin buffer type definitions are detailed in the Buffer Types section.

Table 2-5. MII/SC-MII/RMII Signals
NameSymbolBuffer TypeDescription
Transmit Data 0TXD0

VIS-VDDP

PD

Transmit data bus bit 0 (all modes).

Transmit Data 1TXD1

VIS-VDDP

PD

Transmit data bus bit 1 (all modes).

Transmit Data 2

(MII/SC-MII modes)

TXD2

VIS-VDDP

PD

Transmit data bus bit 2 (MII/SC-MII modes).

In RMII mode, this signal is not used and is internally pulled-down to VSS.

Transmit Data 3

(MII/SC-MII modes)

TXD3

VIS-VDDP

PD

Transmit data bus bit 3 (MII/SC-MII modes).

In RMII mode, this signal is not used and is internally pulled-down to VSS.

Transmit Error

(MII mode)

TXER

VIS-VDDP

PD

This input is asserted to indicate that an error was detected somewhere in the packet presently being transferred to the device.

This pin is unused in RMII mode and should be connected to VSS if it is not used for ACMA functionality on the LAN8670.

This pin is shared with the ACMA functionality on the LAN8670.
Transmit EnableTXEN

VIS-VDDP

PD

Indicates that valid transmission data is present on TXD[3:0]. In RMII mode, only TXD[1:0] provide valid data.

Note: A pull-down resistor is recommended to prevent incidental transmission if the MAC does not actively pull-down or drive this pin low at all times during its reset and initialization.
Transmit Clock

(MII mode)

TXCLKVO-VDDP

2.5 MHz clock used to latch data from the MAC into the device.

In RMII mode, this pin is unused and is driven low. It should be left unconnected if it is not used for RXPI functionality on the LAN8670.

This pin is shared with the RXPI functionality on the LAN8670.

Receive Data 0RXD0VOH-VDDP

Receive data bus bit 0 (all modes).

This pin shares functionality as a PHYAD2 configuration strap and, therefore, must be connected to VDDP/VSS through a pull‑up/pull‑down resistor, as desired.

Receive Data 1RXD1VOH-VDDP

Receive data bus bit 1 (all modes).

This pin shares functionality as a PHYAD3 configuration strap and, therefore, must be connected to VDDP/VSS through a pull‑up/pull‑down resistor, as desired.

Receive Data 2

(MII/SC-MII modes)

RXD2VO-VDDP

Receive data bus bit 2 (MII/SC-MII modes)

This pin shares functionality as a MODE0 configuration strap and, therefore, must be connected to VDDP/VSS through a pull‑up/pull‑down resistor, as desired.

When the LAN8670 is configured for RMII operation, the RXD2 signal is unused.

Receive Data 3

(MII/SC-MII modes)

RXD3VO-VDDP

Receive data bus bit 3 (MII/SC-MII modes).

This pin shares functionality as a MODE1 configuration strap and, therefore, must be connected to VDDP/VSS through a pull‑up/pull‑down resistor, as desired.

When the LAN8670 is configured for RMII operation, the RXD3 signal is unused.

Receive ErrorRXERVOH-VDDP

This output is asserted to indicate that an error was detected somewhere in the packet presently being transferred from the device.

This signal is optional in RMII mode and may be left unconnected from the MAC. This pin shares functionality as a PHYAD0 configuration strap, however, and, therefore, must be connected to VDDP/VSS through a pull‑up/pull‑down resistor, as desired.

Receive Data Valid

(MII/SC-MII modes)

RXDVVOH-VDDP

Indicates that recovered and decoded data is available on the RXD[3:0] pins.

This pin shares functionality as a PHYAD1 configuration strap and, therefore, must be connected to VDDP/VSS through a pull‑up/pull‑down resistor, as desired.

When the LAN8670 is configured for RMII operation, the RXDV signal is unused. The pin, however, is used as CRSDV.

Receive Clock

(MII mode)

RXCLKVO-VDDP

In MII mode, this pin is the 2.5 MHz receive clock output.

In RMII mode, this pin is unused and is driven low. It should be left unconnected if it is not used for WAKEOUT functionality on the LAN8670.

This pin is shared with the WAKEOUT functionality on the LAN8670.

Single Media Clock

(SC-MII mode)

SMCLKVO-VDDP

In Single Clock MII mode, this pin is the 2.5 MHz clock output to be connected to the media access controller MII TXCLK and RXCLK input pins.

This pin is shared with the WAKEOUT functionality on the LAN8670.

Carrier Sense / Receive Data Valid (RMII mode)CRSDVVOH-VDDP

This signal is asserted to indicate the receive medium is non-idle in RMII mode.

This pin shares functionality as a PHYAD1 configuration strap and, therefore, must be connected to VDDP/VSS through a pull‑up/pull‑down resistor, as desired.

When the LAN8670 is configured for MII or SC-MII operation, the CRSDV signal is unused. The pin, however, is used as RXDV.

Collision Detect

(MII/SC-MII modes)

COLVO-VDDP

Collision Detect.

In RMII mode, this pin should be connected to VSS as it is unused and floating.

Carrier Sense

(MII/SC-MII modes)

CRSVO-VDDP

Carrier Sense.

This pin shares functionality as a PHYAD4 configuration strap and, therefore, must be connected to VDDP/VSS through a pull‑up/pull‑down resistor, as desired.

Table 2-6. Ethernet Transceiver Pins
NameSymbolBuffer TypeDescription
Ethernet TX/RX Positive TerminalTRXPAIOPositive terminal for transmit/receive signal.
Ethernet TX/RX Negative TerminalTRXNAIONegative terminal for transmit/receive signal.
Table 2-7. Serial Management Interface (SMI) Pins
NameSymbolBuffer TypeDescription
SMI Data Input/OutputMDIO

VIS-VDDP /

VO-VDDP

Serial Management Interface data input/output. Should be connected to VDDP via pull-up resistor.
SMI ClockMDCVIS-VDDPSerial Management Interface clock.
Table 2-8. Power Management Pins
NameSymbolBuffer TypeDescription
InhibitINHVODH-VDDAU

Inhibit. Used to switch on/off the main external voltage regulators.

This pin operates in the VDDAU domain.

RESET_N assertion does not affect the state of this pin.

This signal is an active high P-channel open-drain source output. The pin will be driven to VDDAU to inhibit the shutdown of external voltage regulators. When the external regulators may be shutdown, this pin will become high impedance.

Note: When used, this pin requires a pull-down resistor.

When not used, this pin should be left unconnected.

Wake InputWAKE_INVI-VDDAU

Wakeup Input. Asserted to move the part out of sleep.

Note: This pin operates in the VDDAU domain.
Note: When used, this pin requires a pull-up or pull-down resistor, depending on the software configured assertion polarity. If a pull-up is used, it must be connected to VDDAU.

When not used, this pin should be connected to VSS.

Wake OutputWAKE_OUTVO-VDDP

Wake Output. Asserted when the part wakes out of sleep.

Note: When used, this pin requires a pull-down resistor.
Note: This pin operates in the VDDP domain.

When not used, this pin should be left unconnected.

Table 2-9. Application Pins
NameSymbolBuffer TypeDescription
Application Controlled Medium AccessACMAVIS-VDDPApplication Controlled Medium Access. When this feature is enabled, the station controller may assert this input to allow the PHY to transmit to the medium.

When unused, this pin is an input and should be connected to VSS.

Receive Packet IndicationRXPIVO-VDDPReceive Packet Indication. This pin is asserted by the Time Synchronization block to indicate the reception of a packet. This pin may also be asserted when the PHY receives a packet that matches a configured pattern. The packet matching feature is typically used to trigger on reception of IEEE Std 802.1AS gPTP packets.

When unused, this pin is actively driven low and may be left unconnected.

Transmit Packet IndicationTXPIVO-VDDPTransmit Packet Indication. This pin is asserted by the Time Synchronization block to indicate the transmission of a packet. This pin may also be asserted when the PHY transmits a packet that matches a configured pattern. The packet matching feature is typically used to trigger on transmission of IEEE Std 802.1AS gPTP packets.
General Purpose Application I/OGPIO0VIS-VDDP /

VO-VDDP

General Purpose Application I/O 0. This pin may be configured as ACMA, TXPI, RXPI, or RXTXPI.

The station management entity cannot directly drive or read this pin through CSR writes or reads.

When unused, this pin is actively driven low and may be left unconnected.

Table 2-10. Miscellaneous Pins
NameSymbolBuffer TypeDescription
External 25 MHz Crystal InputXTIICLKExternal 25 MHz crystal input (MII/SC-MII only).
External 25 MHz Crystal OutputXTOOCLKExternal 25 MHz crystal output (MII/SC-MII only).
Note: When the LAN8670 is in RMII mode, this pin should be left unconnected.
External Clock InputREFCLKINICLK50 MHz, 1.8-3.3V single-ended clock oscillator input (RMII only).
InterruptIRQ_NVODL-VDDPDevice interrupt request. Active low N-channel open-drain sink output.
Note: This pin requires a 10 kΩ (typical) pull-up to VDDP.
System ResetRESET_N

VIS-VDDP

PU

System reset. This pin is active low.

If unused, this pin may be connected directly to VDDP.

Bias ResistorRBIASAIOExternal bias resistor connection pin. This pin requires connection of a 12.4 kΩ resistor to ground.
Note: The resistor must be within ± 1% tolerance across the entire expected operating temperature range.
Do Not ConnectDNC-The pin must be left floating externally unless otherwise directed by Microchip.
Table 2-11. Configuration Straps
NameSymbolBuffer TypeDescription
Operating Mode Configuration Straps 1-0MODE[1:0]VIS-VDDPThese configuration straps are used to select the device’s default mode of operation. See Configuration Straps for additional information.
Note: These pins must be connected to either VDDP or VSS via a pull-up/pull-down resistor (10 kΩ, typical) to configure the desired operating mode.
PHY Address Configuration Straps 4-0PHYAD[4:0]VIS-VDDPThese configuration straps are used to select the device’s default PHY SMI address. See Configuration Straps for additional information.
Note: These pins must be connected to either VDDP or VSS via a pull-up/pull-down resistor (10 kΩ, typical) to configure the desired SMI address.
Table 2-12. Power Pins
NameSymbolDescription
+3.3V Switchable I/O Power Supply InputVDDP+3.3V I/O power supply input. When in sleep mode, this supply must be disabled.
+3.3V Continuous VDDAU Power Supply InputVDDAU+3.3V continuous VDDAU power supply input.
Note: This supply must be provided during sleep mode.
Note: When wake/sleep support is not used, this pin is connected to the same supply as VDDA.
+3.3V Switchable Analog Power Supply InputVDDA+3.3V analog power supply input. When in sleep mode, this supply must be disabled.
GroundVSSCommon ground.
Note: This exposed pad must be connected to the ground plane with a via array.