2 Data Logging

Obtaining clear data is helpful for review. Even if the issue is not well understood, there are common logs that are always useful to have available.

Note: If submitting a support case through Microchip’s support portal, include these logs in the support case attachments.

Collect the following information during the debug process. This information will be critical in diagnosing and debugging any issue. If you are filing a support case through Microchip Support, gather the following information in advance. This preparation will help speed up the response time, as the Microchip engineer will likely request all of these items during the initial correspondence.

Table 2-1. Recommended Data Logs for Collection
ItemNotesHow-to
Collect device register dump.Also summarize, in writing, what settings are intended to be modified/set.The driver may need to be instrumented to execute raw register read/write commands, refer to the driver information for these commands.
Schematic of KSZ8081RNB and all schematic pages which the KSZ8081RNB signals route to.A searchable ‘.pdf’ file is the most useful format. Image files are not recommended.n/a
Layout of KSZ8081RNB and all portions of the layout which the KSZ8081RNB signals route to.Native design program files are most useful. Native Gerber files are also useful but less preferred. Images and ‘.pdf’ files of Gerbers are difficult to review and not desirable.n/a
Ethernet Wireshark trace (use a WireShark Tap if you cannot run Wireshark on your system)Save the protocol trace file in native format.n/a