10.2 Device Firmware Upgrade Over Serial
Device Firmware Upgrade(DFU) over serial is the functionality in Bootloader that user uses it to load new image received over serial interface and write into the flash. PC GUI tool(MicrochipUtilityTool.exe) and Python Script are two methods used for DFU over serial. The following application guide and demonstration steps use these two methods to carry out the DFU over serial. The demonstration is to upgrade ble_sensor user application with a new image.
DFU over Serial Using Microchip Utility Tool
MicrochipUtility is a GUI tool, it suppors OTAU over serial, Zigbee OTAU. The utility tool is provided in Microchip website Microchip Utility Tool. For the application guide and demonstration using this tool for the serial DFU, go to Serial Bootloader Demo
DFU over Serial Using Python Script
Pre-requisite:
ble_sensor project as current user application(version 1.0.0.0):
wireless_apps_pic32cxbz3_wbz35\apps\ble\advanced_applications\ble_sensor\firmwarePrecompiled ble_sensor new image(binary file):
wireless_apps_pic32cxbz3_wbz35\apps\ble\advanced_applications\ble_sensor\precompiled_hex\ble_sensor.X.production.signed_uart_1.0.0.1.binBootloader:
-
Precompiled hex file for GPIO Trigger mode DFU:
wireless_apps_pic32cxbz3_wbz35\apps\bootloader\bootloader\precompiled_hex\bootloader.X.production.he -
Precompiled hex file for Timer Based Trigger DFU:
wireless_apps_pic32cxbz3_wbz35\apps\bootloader\bootloader\precompiled_hex\bootloader_timer.X.production.hex
-
-
Python Script Files:
- For GPIO Trigger mode DFU: flash_load_2ndSlot.py, progctrl.py
(wireless_pic32cxbz_wbz\utilities\pic32cx-bz\dfuPythonScripts\) - For Timer Based Trigger DFU: flash_load_2ndSlot_timer.py,
progctrlOptimized.py
(wireless_pic32cxbz_wbz\utilities\pic32cx-bz\dfuPythonScripts\)
- For GPIO Trigger mode DFU: flash_load_2ndSlot.py, progctrl.py
Hardware: WBZ351 Curiosity board
Running a Python Script:
For GPIO Trigger DFU, execute python script using the following command:
python flash_load_2ndSlot.py -i image.bin
For Timer Based Trigger DFU, execute python script by using the following command:
python flash_load_2ndSlot_timer.py -i image.bin
image.bin is the binary file of new user image, this binary file is generated from user application by MPLAB X IDE. It could be other file name from user’s own application, it may have path name before the file.
DFU over Serial Demonstration:
Following are steps to operate DFU over seiral, programing a new user image by using Bootloader.
Preparation: Create and Program Unified image

Then on the IDE Tools bar, click Clean and Build Main Project icon to build the project. Since the project has a loadable hex file added, code building will create a unified image hex file ble_sensor.X.production.signed.unified.hex
Program Unified Image to Board
ble_sensor.X.production.signed_uart_1.0.0.1.binFor creating unified image, refer to Bootloader - section Configure User Application to use Bootloader - Add Bootloader as Lodable File/Project to Create Unified Image to know more details.
Enter into DFU Mode
For the provided bootloader example, DFU mode is triggered by SW2 Button on WBZ351 Curiosity board. So press and hold SW2 Button first, then short press Reset button(SW1) to restart the firmware, the firmware will enter DFU mode. Opening Tera Term on PC, and configure it as 115200/8bit/none Parity/1 Stop bit, will see the message output as “DFU Now!”.
Display Message "DFU Now!" in Tera Term

This message means the board is under DFU mode.
Run Python Script to do DFU
Close Tera Term and open Windows Command Prompt, go to the directory where python script files and binary image file are located and execute python script as below:
python flash_load_2ndSlot.py -i ble_sensor.X.production.signed_uart_1.0.0.1.bin
To run above python script, user may need to copy those python script files and binary image file into a same folder. However, python script also support file with aboslute path name or relative path name.
Execute Python Script and see DFU Progress

python flash_load_2ndSlot_timer.py -i ble_sensor.X.production.signed_uart_1.0.0.1.bin
Execute Python Script, Reset Board, and see DFU Progress

The % progress will tell the DFU progress. Once it is finished as 100%, the new image is copied to slot1 of internal flash memory.
Reset Board to Start New Firmware
Python script has not supported firmware automatical reboot after DFU completion, so need manually reset the board to start new firmware.
Once DFU progress achieves 100% complete, close Windows Command Prompt and open Tera Term to see the message output. On the board, press the Reset button(SW1) to restart, the bootloader will then copy new firmware from flash memory slot1 to slot0. After that, bootloader will jump and start new user image in slot0. On Tera Term, user will see messages as shown below, original firmware version is 1.0.0.0, now firmware version is 1.0.0.1, the DFU is successful.
Display Message About Firmware Erase/Copy/Verify in Tera Term