4.2.1.2 Uploading and Creating bin File for PFM OTA DFU
The following BLE OTA demo steps are common for any application implementing OTA functionality.
BLE sensor application is the sample project which implements OTA functioanlity as
explained in the above steps. The current image
(ble_sensor.X.production.signed.unified_gpiobased.hex or
ble_sensor.X.production.signed.unified_timerbased.hex) with OTA
capability and new upgradable .bin (ble_sensor_1.0.0.1_enc_ota.bin) is also available
in \ble\advanced_applications\ble_sensor\precompiled_hex for your
reference.
-
Hardware Requirement:
|
Tool |
Qty |
| WBZ351 Curiosity Board |
1 |
|
Micro USB cable |
1 |
|
Android/iOS Mobile |
1 |
-
Smartphone App: Microchip Bluetooth Data (MBD) iOS/Android app available in stores
-
Demo steps:
- To perform the OTAU, the
upgradable firmware bin file has to be created and must be stored in the MBD
app. To create the upgradable firmware bin file , the following changes in
Project Properties must be done after creating the project graph.
Figure 4-55. Project Properties - Header configuration Figure 4-56. Project Properties - OTA configuration After the Project Properties configurations, click on Create OTA File. The Upgradable .bin image with selected "Output File Name" will be created in .X folder. This is the image stored in OTAU Manager to send to OTAU Target.
- Send the upgrdable bin file
to the mail. Refer to the following screenshots to store the image received
on mail into MBD app.
-
Android Mobile:
Download the .bin file that was sent over email
Downloading the .bin file open the downloaded .bin file with MBD Save the file in MBD by selecting "SAVE FILE" -
- Turn on mobile Bluetooth and select “OTA DFU" tab of Microchip
Bluetooth Data App on the mobile device.

- Power On the OTA capable
target device (PIC32CXBZ3/WBZ35) which was
programmed in "Programming the
Application using MPLABX IDE". Device will be advertising. Click
on "SCAN" button in mobile app and the device be visible in scanned list.
Click on intended device from the scanned list. Mobile app will now get
connected with OTA Target device.
- "Connected" message will
appear for a short while. Click the ‘Select Image’ option to choose the
available firmware file.
- The OTAU firmware image file
copied in the step 1 will be visible on screen. Click on that image.
- After confirming the FW
version press OK button.
- Firmware update will be initiated and the progress will be shown in mobile
app. The process would take few seconds.
- Once the complete image is transferred, "OTA Update successfully" status
will be shown in mobile app. Click on "OK" and then device will perform
authentication of the image. If validation is successful, then system reboot
automatically.
- On bootup, device does the authentication of new image in Slot1 and then copies the new image to Slot0. Now the new image will be running from Slot0.
- To verify whether the running image on the target is newly upgraded image, follow steps 2 to 7 and check the current version.
- To perform the OTAU, the
upgradable firmware bin file has to be created and must be stored in the MBD
app. To create the upgradable firmware bin file , the following changes in
Project Properties must be done after creating the project graph.