Service Behaviors
Disconnection Behavior
When this service is instantiated in a device and the connection is lost for any reason, the device shall start alerting to the current link loss alert level.
If the current link loss alert level is “No Alert,” no alerting shall be done on this device.
If the current link loss alert level is “Mild Alert,” the device shall alert.
If the current link loss alert level is “High Alert,” the device shall alert in the strongest possible way.
The specific action that occurs in the device for the mild and high alerts is implementation specific.
For example, this could include flashing lights, making noises, moving, or other methods to alert the user.
This alert continues until one of the following conditions occurs:
- an implementation-specific timeout
- user interaction on this device
- the physical link is reconnected