4.1.2.4 BLE Deep Sleep Advertising
Getting Started with Peripheral Building Blocks
FreeRTOS BLE App Initialize -> BLE Deep Sleep Advertisements
Introduction
This document will help users enable "Deep Sleep" mode with BLE Advertisements on the WBZ351 Curiosity board using the MPLAB Code Configurator (MCC). In this application example, the Deep Sleep advertisement interval will be set to 1 second. This interval dictates the application Deep Sleep time.
Users of this document can choose to just run the precompiled Application Example hex file on the WBZ351 Curiosity board and experience the demo or can go through the steps involved in developing this application from scratch.
These examples each build on top of one another. We strongly recommend that you follow the examples in order, to learn the basics concepts first before progressing to the more advanced topics.
Recommended Reads
Hardware Required
Tool | Qty |
---|---|
WBZ351 Curiosity Board | 1 |
Micro USB cable | 1 |
Android/iOS Smartphone | 1 |
Optional Power Debugger/Multimeter/Oscilloscope to measure power
SDK Setup
Software
TeraTermSmartphone App
Microchip Bluetooth Data (MBD) iOS/Android app available in stores
Programming the precompiled hex file or Application Example
Programming the hex file using MPLABX IPE
-
Import and program the Precompiled Hex file:
<Harmony Content Path>\wireless_apps_pic32cxbz3_wbz35\apps\ble\building_blocks\peripheral\deep_sleep_adv\hex\deep_sleep_adv.X.production.signed.hex
- For more details on the steps, go to Programming A DeviceNote: Ensure to choose the correct Device and Tool information
Programming the Application using MPLABX IDE
- Follow the steps mentioned in Running a Precompiled Example
- Open and program the Application:
<Harmony Content Path>\wireless_apps_pic32cxbz3_wbz35\apps\ble\building_blocks\peripheral\ deep_sleep_adv\firmware\deep_sleep_adv.X
For more details on how to find the Harmony Content Path, refer to Installing MCC Plugin
Demo Description
This application example enables users to enter Deep Sleep mode while transmitting Connectable, Undirected BLE Advertisements. On power-on reset, the application will enter Deep Sleep mode. When USR-BTN2 (SW2) is pressed, the device on-board GREEN LED starts blinking to denote the start of advertisements. The device will then enter Deep Sleep mode periodically based on the advertisement interval of 1 second. When the device connects with the mobile app, the onboard LED starts to glow solid, which indicates that the connection is established and the device will enter Standby Sleep mode during Idle state.
Testing
- Using a micro USB cable, connect the Debug USB on the Curiosity board to a PC
- Program the precompiled hex file or application example as mentioned. Upon flashing, there will be no indication on the board since the device entered Deep Sleep mode.
- Press SW2 on the board to start Deep Sleep Advertising
- Launch the MBD mobile app and select the BLE Smart sub app to see the scan results. Device name "BLE_DSADV" should appear.
Current Consumption Measurement
Connect a Multimeter/Power Debugger/Oscilloscope to Power Measurement Header J6. If using a Power Debugger, users can use Data Visualizer to measure the current consumption.
Current measured in Deep sleep mode is around 1.9 uA.
Current measured in Deep sleep + Advertising mode is around 130 uA average.
Users of this early adopter package should go through the known issues document and understand the limitations, if any, with the current low power mode implementation.
Developing the application from scratch
There are two possible ways to develop this application. In the following section, users can make use of the import method available in the MPLAB Code Configurator (MCC). This is the easiest and quickest way to recreate the application with the help of an import component configuration. In the second section, users can experience the complete application development from scratch using the MCC.
Developing this Application using MPLAB Code Configurator Import method
This section explains the steps required by a user to develop this application example from scratch using the MPLAB Code Configurator
-
Create a new MCC Harmony Project
- To setup the basic components and configuration required to develop this
application, import component configuration:
<Harmony Content Path>\wireless_apps_pic32cxbz3_wbz35\apps\ble\building_blocks\peripheral\deep_sleep_adv\firmware\deep_sleep_adv.X\deep_sleep_adv.mc3
For more details, refer to Import existing App Example ConfigurationNote: Import and Export functionality of the Harmony component configuration will help users to start from a known working setup of the MCC configuration -
To accept dependencies or satisfiers, select "Yes".
-
Verify if the Project Graph window has all the expected configuration.
Developing this Application from scratch using MPLAB Code Configurator
-
Create a new MCC Harmony Project
- In the previous step, the BLE
Stack component is included. Accept all the component auto-activations and
attachment auto-connect confirmations.
- Include the RCON Component from
the peripheral category.
-
Include the Transparent Service and Transparent Profile component located at :Harmony-> Wireless->Drivers->BLE
-
Establish the link between the Transparent Service and Profile components
-
Click on the Transparent Profile component. In the configuration option, enable server role
- Click on the BLE Stack component.
In the configuration option, enable sleep mode
- This action will trigger the auto inclusion of the RTC component. Accept the
activations and auto-connect confirmations.
-
Final Project graph with all the required component
Verify Advertisement and Component Configuration
This section details the configuration changes needed for each component in accordance with the application use case implementation.
- Select the BLE_Stack
component in the project graph
Note: Advertising Interval Min can be modified to adjust Deep Sleep Advertising interval
Tip: Advertisement payload can be configured by user here
- Select clock
configuration.
- Configure RTC clock configuration.Note: Even after enabling and selecting the SOSC as backup source in the clock configuration, the LPCLK and RTC clock still show as 0Hz. This is a known issue which will be resolved in the upcoming MCC release. For the time being, to fix this issue, a manual application code modification is necessary. The required change will be discussed in the next section.
- Configure LED GPIO Configuration.
Note: The above GPIO configuration is used for indicating the device state in this example and is optional
Tip: The configuration bits will be generated after user Generates Code
-
Configure RTOS configuration by increasing the Total heap size from the default value
Generate Code
For more details on code generation, refer to MPLAB Code Configurator (MCC) Code Generation
Files and Routines Automatically generated by the MCC
After generating the program source from the MCC interface by clicking Generate Code, the BLE configuration source and header files can then be found in the following project directories.

The OSAL, RF System and BLE System initialization routine executed during program initialization can be found in the project file. This initialization routine is automatically generated by the MCC.

The BLE stack initialization routine executed during Application Initialization can be found in project files. This initialization routine is automatically generated by the MCC. This call initializes and configures the GAP, GATT, SMP, L2CAP and BLE middleware layers.
During system sleep, clock (system PLL) will be disabled and system tick will be turned off. FreeRTOS timer needs to be compensated for the time spent in sleep. RTC timer which works in sleep mode is used to accomplish this. RTC timer will be initialized after BLE stack initialization.

Source Files | Usage |
---|---|
app.c | Application State machine, includes calls for Initialization of all BLE stack (GAP,GATT, SMP, L2CAP) related component configurations |
app_ble.c | Source Code for the BLE stack related component configurations, code related to function calls from app.c |
app_ble_handler.c | All GAP, GATT, SMP and L2CAP Event handlers |
app_ble_dsadv.c | Source Code for utilizing the deep sleep advertising functionality |
device_deep_sleep.c | Source Code for deep Sleep and wake up related system configurations |
Tip: app.c is autogenerated and has a state machine-based application code sample. Users can use this template to develop their own application.
Header Files
-
ble_gap.h
contains BLE GAP functions and is automatically included inapp.c
Function Calls
- MCC generates and adds the code to initialize the BLE Stack GAP, GATT, SMP and L2CAP in APP_BleStackInit() and the Deep Sleep Advertising functionality in APP_BleDsadvStart(flag)
- APP_BleStackInit() and APP_BleDsadvStart(flag) are the APIs that will be called
inside the Applications Initial State APP_STATE_INIT in
app.c
Manual Application code edit
This section talks about the mandatory code modifications that need to be incorporated in order to implement the Deep Sleep Advertising functionality.
Step 1: app_user_edits.c
- Some of the Harmony 3 generated
files cannot be fully configured by the MPLAB Code Configurator. This file
contains the instructions for the user to modify these files.
Follow the instruction mentioned in
app_user_edits.c
and after completing the required edits, comment out or remove the #error line
Step 2 - Initialization.c
- Comment the code inside
SYS_Initialize function
In the MCC Generated Code, the CLK_Initialize() and ROM functions are by default present inside the SYS_Initialize() function. The user needs to comment out the code referring to CLK_Initialize() and ROM functions in the SYS_Initialize() function and should add under _on_reset() function in same
initialization.c
file.
- Code Inclusion inside
_on_reset function
The previously commented code inside SYS_Initilaze() function is included here
CLK_Initialize(); typedef int (*FUNC_PCHE_SETUP)(uint32_t); ((FUNC_PCHE_SETUP)(*(uint32_t*)0xF2D0))((PCHE_REGS->PCHE_CHECON & (~(PCHE_CHECON_PFMWS_Msk | PCHE_CHECON_ADRWS_Msk | PCHE_CHECON_PREFEN_Msk))) | (PCHE_CHECON_PFMWS(2) | PCHE_CHECON_PREFEN(1))); //Set RF as idle mode RF_SetIdleMode();
- Code Inclusion inside
SYS_Initialize function
DEVICE_DeepSleepWakeSrc_T wakeSrc; DEVICE_GetDeepSleepWakeUpSrc(&wakeSrc); if (wakeSrc == DEVICE_DEEP_SLEEP_WAKE_NONE) //Initialize RTC if wake source is none(i.e power on reset) { RTC_Initialize(); }
Step 3 - heap_4.c
- Comment the below code and replace it with the Modified Code inside heap_4.c (available as part of FreeRTOS-->MemMang)
static uint8_t ucHeap[ configTOTAL_HEAP_SIZE ]; --> Original Code
static uint8_t __attribute__((section (".bss.ucHeap"), noload)) ucHeap[ configTOTAL_HEAP_SIZE ]; -->Modified Code
Step 4 - Plib_rtc.h
- Default generated: #define RTC_COUNTER_CLOCK_FREQUENCY (0U / (1UL << (0x1U - 1U)))
- Replace to: #define RTC_COUNTER_CLOCK_FREQUENCY (32768U / (1UL << (0x1U - 1U)))
Step 5 - Plib_clk.c
- To enhance the CLK initialization period for the delay time of polling XTAL and PLL ready, mentioned below are changes that need to be made. This requires a manual code change as the current MCC is not capable of generating the required code.
- MCC Present Setting
- MCC New Settings
//check CLDO ready
while ((CFG_REGS->CFG_MISCSTAT & CFG_MISCSTAT_CLDORDY_Msk) == 0);
//programming 4ms delay - programming subsys_xtal_ready_delay -> Reduce to 2ms
//check xtal spec for delay required
BTZBSYS_REGS->BTZBSYS_SUBSYS_CNTRL_REG1 = ((BTZBSYS_REGS->BTZBSYS_SUBSYS_CNTRL_REG1 & ~BTZBSYS_SUBSYS_CNTRL_REG1_subsys_xtal_ready_delay_Msk)
| ((0x01) << BTZBSYS_SUBSYS_CNTRL_REG1_subsys_xtal_ready_delay_Pos));
//wait for crystal ready
while((BTZBSYS_REGS->BTZBSYS_SUBSYS_STATUS_REG1 & BTZBSYS_SUBSYS_STATUS_REG1_xtal_ready_out_Msk) != BTZBSYS_SUBSYS_STATUS_REG1_xtal_ready_out_Msk);
// set PLL_enable
BLE_REGS->BLE_DPLL_RG2 &= ~(0x02);
//programming delay for pll lock - 500 us -> Reduce to 64us
//32 us steps - check pll spec for final value
BTZBSYS_REGS->BTZBSYS_SUBSYS_CNTRL_REG3 = ((BTZBSYS_REGS->BTZBSYS_SUBSYS_CNTRL_REG3 & ~BTZBSYS_SUBSYS_CNTRL_REG3_subsys_pll_ready_delay_Msk )
| ((0x02) << BTZBSYS_SUBSYS_CNTRL_REG3_subsys_pll_ready_delay_Pos));
Step 6 - WBZ351.ld
- Additional linker file related changes need to be incorporated to define the backup RAM address. This configuration will be later made available in the MCC configuration. Until then, this manual edit is required.
- The highlighted code in the below image needs to be incorporated to the MCC
generated
WBZ351.ld
file
User Application Development
Include
-
definitions.h
must be included in all the files where port pin macros are used
Note:definitions.h
is not specific to just port peripheral but instead must be included in all the application source files where any peripheral functionality will be exercised
Enter Deep Sleep mode
- DEVICE_EnterDeepSleep(false,0);
This API can be called to put the device to Deep Sleep mode.
Start Deep Sleep Advertisement
- APP_BleDsadvStart(false);
This API can be called in APP_STATE_INIT of
app.c
to start the Deep Sleep AdvertisingNote: Users can exercise other various BLE Advertisement functionalities by using the BLE Stack APIs
Application Use Case Implementation
This application implementation is purely user choice. It is designed in such a way that the device enters into Deep Sleep mode upon power up and when SW2 is pressed, the device starts the Deep Sleep Advertisements based on the fixed advertisement interval. Device then wakes up from Deep Sleep in regular intervals to start an advertisement and go back to sleep again.
This scenario is implemented by modifying the default generated code inside the
switch case in app.c
. User can implement their desired
application workflow by making use of the available function calls.
Known Issue:
System Sleep implementation source (device_sleep.c
) and header
(device_sleep.h
) files may sometimes not be included when
generating the project through MCC so follow the below steps to avoid this.
Step1: Uncheck and re-enable the Enable Sleep Mode and Enable Deep Sleep Advertising option inside the BLE Stack component in the project graph as shown in the figure below and accept the dependencies requested.

Step2: Click the Force Update on All option and press Generate