AC PWM Generation | This example application shows
how to use the Analog Comparator Peripheral library to generate a 1
kHz PWM waveform |
AC Sleepwalking | This example application shows
how to use the AC Peripheral library to perform a single shot
comparison in standby sleep mode periodically and wake up the device
at the end of a successful comparison |
ADC DMA Sleepwalking | This application shows how to
configure the ADC in a sleepwalking operation, where the input
voltage is measured at a fixed interval, and then the device is
woken from sleep after conversion of 16 samples |
ADC Sample | This example application shows
how to sample an analog input using the ADC and displays the
converted samples on a serial terminal |
ADC Window Sleepwalking | This application shows how to
configure ADC in a sleepwalking operation, where input voltage is
measured at a fixed interval, but device is not woken from sleep
until the measured value is below a given threshold |
Clock Configuration | This example application shows
how to configure the clock system to run the device at maximum
frequency. It also outputs a prescaled clock signal on a GPIO pin
for measurement and verification |
DAC Waveform Generation | This example application shows
how to use the DAC to generate a 1 kHz Sine or Sawtooth wave with a
look up table |
DAC Waveform Generation with DMA | This example application shows
how to use the DAC with the DMA to generate a 5 kHz sinusoidal
waveform without CPU intervention |
DMAC Memory Transfer | This example application
demonstrates how to use the DMAC peripheral to do a memory to memory
transfer |
DMAC USART Echo | This example application
demonstrates USART transfer with DMA to receive 10 bytes and echo
back the received bytes |
DSU Compute CRC32 | This example application
demonstrates how to use the DSU Peripheral library to compute 32-bit
Cyclic Redundancy Checksum (CRC) |
EIC Interrupt | This example application
demonstrates how to generate interrupt using the EIC on switch press
and indicate it through an LED |
NVMCTRL Read Write | This example application
demonstrates how to use the NVMCTRL to erase and program the
internal Flash memory |
PM Wakeup Using RTC | This example demonstrates
entering the low power modes and exiting it using the RTC |
PORT Polling | This example application
demonstrate how to poll the switch input, and indicate the switch
status using the LED |
RTC Alarm Interrupt | This example shows how to use the
RTC to configure the time and generate the alarm |
RTC Periodic Interrupt | This example application shows
how to use the RTC to generate periodic interrupts |
SERCOM I2C EEPROM Emulation (I2C
Client) | This example application
demonstrates how to use the SERCOM peripheral in client mode |
SERCOM I2C EEPROM Read Write | This example application
demonstrates how to use the SERCOM peripheral to write and read from
the I2C serial EEPROM memory |
SERCOM SPI Blocking | This example application
demonstrates how to use the SERCOM SPI peripheral to transmit and
receive a block of data in a blocking manner |
SERCOM SPI EEPROM Read Write | This example application
demonstrates how to use the SERCOM SPI peripheral to write and read
from the SPI serial EEPROM memory |
SERCOM SPI Interrupt | This example application shows
how to use SERCOM SPI PLIB with external loop back to write and then
read back an array of data in interrupt mode |
SERCOM SPI Ping Pong with DMA | This example demonstrates how to
continuously transmit and receive data over a SPI interface using
ping pong buffers with DMA |
SERCOM USART Blocking | This example application
demonstrates how to use the SERCOM peripheral in USART mode to
transfer block of data in a blocking manner |
SERCOM USART Interrupt | This example application
demonstrates how to use the SERCOM peripheral in USART mode to
transfer data in a non-blocking manner |
SERCOM USART Ring Buffer | This example application
demonstrates how to use the SERCOM peripheral in USART ring buffer
mode to transfer data in a non-blocking manner |
Systick Periodic Interrupt | This example shows how to use the
SysTick to generate periodic interrupts |
TC Capture Mode | This example shows how to use the
TC module in capture mode to measure duty cycle and frequency of an
external input |
TC Compare Mode | This example shows how to use the
TC module in compare mode to generate an active low, active high,
and toggle output on compare match |
TC Timer Mode | This example shows how to use the
TC module in timer mode to generate periodic interrupt |
TCC PWM Generation | This example application shows
how to use the TCC to generate a 2 or 3 phase PWM signals for motor
control with dead time |
WDT Timeout | This example shows how to
generate a Watchdog timer reset by emulating a deadlock |