PD-9001GS Midspan does not power up | - Verify that an approved power cord is used.
- Verify that the voltage at the power inlet is between 100 and 240 VAC.
- Remove and re-apply power to the device and check the indicators during the power-up sequence.
|
The Powered Device (PD) does not operate | - Verify that the PD is designed for PoE operation according to IEEE® 802.3at standard.
- Verify that you are using a standard, straight-wired four-pair cable (UTP/FTP Category 5/5e/6).
- Verify that the PD is connected to the PD-9001GS "Terminal" port.
- If an external power splitter is in use, replace it with a known-good splitter.
- Remove and re-apply power to the Midspan.
|
The end device operates, but there is no data link | - Verify that you are using a standard straight-wired, four-pair cable (UTP/FTP Category 5/5e/6).
- Verify that the Ethernet cable length is less than 100 meters from the Ethernet source to the load/remote terminal.
- Ensure that the input Ethernet cable is connected to the power injector’s "Ethernet" port.
- If an external power splitter is in use, replace it with a splitter known to be good.
|