13.4 Approved Antenna Types

The ATWILC3000-MR110UA is tested and approved to use with the antennas listed in following table. It is permissible to use a different antenna, provided the same antenna type, antenna gain (equal or less than), similar in-band and out-of-band characteristics (refer to specification sheet for cutoff frequencies).

If other antenna types are used, the OEM installer must authorize the antenna with the respective regulatory agencies and ensure its compliance.

Table 13-2. List of Approved External Antennas
Sl. No.Part NumberManufacturerAntenna Gain @ 2.4GHz BandAntenna TypeATWILC3000-MR110UA(1)Cable Length/Remarks
FCC(2)(3)/ ISEDCE
1W3525B039Pulse Electronics Corporation2 dBiPCBXX100 mm
2RFDPA870920IMLB301WALSIN1.84 dBiDipoleXX200 mm
3RFA-02-P33Aristotle2 dBiPCBXX150 mm
4RN-SMA-SMicrochip0.56 dBiDipoleXXSMA to u.FL cable length of 100 mm (2)(3)
5RFA-02-D3Aristotle2dBiDipoleXX150 mm
6RFA-02-G03Aristotle2dBiMetal StampXX150 mm
7RFA-02-L2H1Aristotle2 dBiDipoleXX150 mm
8RFA-02-P05Aristotle2 dBiPCBXX150 mm
9RFA-02-C2M2Aristotle2 dBiDipoleXXSMA to u.FL cable length of 100 mm (2)(3)
1086254Delock2 dBiPCBX50 mm
Note:
  1. X = Covered under the certification.
  2. If the end product using the module is designed to have an antenna port that is accessible to the end user, then a unique (nonstandard) antenna connector (refer to FCC KDB 353028) must be used; for example, Reverse Polarity – SMA.
  3. If an RF coaxial cable is used between the module RF output and the enclosure, then a unique (nonstandard) antenna connector must be used in the enclosure wall for interfacing with the antenna.
  4. Contact the antenna vendor for detailed antenna specifications to review its suitability to the end-product operating environment and to identify alternatives.

Antenna Placement Recommendations for ATWILC3000-MR110UA

The following recommendations must be applied for the placement of the antenna and its cable:

  • The antenna cable must not be routed over circuits generating electrical noise on the host board or alongside or underneath the module. It is preferable that the cable be routed straight out of the module.
  • The antenna must not be placed in direct contact or in close proximity of the plastic casing/objects.
  • Do not enclose the antenna within a metal shield.
  • Keep any components that may radiate noise, signals or harmonics within the 2.4 GHz to 2.5 GHz frequency band away from the antenna and, if possible, shield those components. Any noise radiated from the host board in this frequency band degrades the sensitivity of the module.
  • It is recommended that the antenna be placed at a distance greater than 5 cm away from the module. The following figure shows the antenna keepout area indication; where the antenna must not be placed in this area.

This recommendation is based on an open-air measurement and does not take into account any metal shielding of the customer end product. When a metal enclosure is used, the antenna can be located closer to the ATWILC3000-MR110UA module.

The drawing provides an option for routing the antenna cable, depending on the location of the antenna with respect to the ATWILC3000-MR110UA PCB. There are two possible options for the optimum routing of the cable.

Figure 13-6. ATWILC3000-MR110UA Antenna Placement Guidelines
Note: These are generic guidelines and it is recommended that customers check and fine-tune the antenna positioning in the final host product based on RF performance.