5.3.30 _Q31sinSeries Function
Generates the sine series with the given normalizing frequency,
f, and the given number of samples, num, starting
from start. Stores the result in buffer, buf.
Include
<libq.h>
Prototype
short _Q31sinSeries(_Q31 f, short start, short num, _Q31
*buf);
Arguments
f | a fixed-point number in Q31 format, which ranges from 0 to (231-1). The valid range of values for this argument is from -1073741824 to 1073741824. The argument represents the Normalizing frequency. |
start | a fixed-point number in Q16 format, which ranges from 0 to (231-1). The valid range of values for this argument is from 1 to 2147483647. This argument represents the Starting Sample number in the Sine Series. |
num | a fixed-point number in Q16 format, which ranges from 0 to
(231-1). The valid range of values for this argument is
from 1 to 2147483647. This argument represents the Number of Sine
Samples the function is called to generate. Note:
num should not be more than 16383 for dsPIC
devices. |
buf | a pointer to the buffer where the generated sine samples would get copied into. |
Return Value
This function returns num, the number of generated sine
samples.