1 Harmony 3 Driver and System Service Application Examples for PIC32MM Family
The following applications are provided to demonstrate the typical or interesting usage models of one or more drivers, system services and RTOS.
| Name | Description |
|---|---|
| Console Debug System Service using UART | This example application demonstrates the UART based console and debug system service |
| FAT File System using NVM Media | This application shows an example of implementing a FAT disk in the device internal Flash memory |
| FAT File System using SDSPI Media | This application shows an example of using the MPLAB Harmony File System to access and modify the contents of a SD card using the SDSPI driver and the SPI PLIB |
| FreeRTOS Basic | This example application demonstrates context switching between different tasks having different priorities |
| I2C Driver Asynchronous - I2C EEPROM | This example application shows how to use the I2C driver in asynchronous mode to perform operations on the EEPROM |
| SPI Driver Asynchronous - Multi Instance | This example demonstrates how to use multiple instances of the SPI driver in asynchronous mode to communicate with multiple EEPROMs |
| Time System Service Multi-client | This example application demonstrates the multi-client system timer functionality |
| USART Driver Asynchronous - USART Echo | This example echoes the received characters over the console using the USART driver in asynchronous mode |
| USART Driver Synchronous - USART Echo | This example echoes the received characters over the console using the USART driver in synchronous mode |