4.5 Revealing More Device Information
Reveal more information about physical drive, array, and logical drive usage in the storage space with the Resources view on the Storage Dashboard.
To reveal physical drives usage by logical drive (and vice-versa), select a controller in the Enterprise View, then open the Resources tab on the Storage Dashboard. The following figure shows that clicking on a logical drive displays its member physical drives and spares; similarly, clicking on a physical drive displays which array (if any) it belongs to. In the following figure, the Device 2 and Device 3 belongs to Array A.