18 Display Properties of a Controller, Array, Logical Device and a Physical Device
This section lists the display properties of a controller, accelerator, array, logical device and physical device.
Property  | Tooltip Details  | 
|---|---|
Model  | Model of the Controller  | 
Status  | The status of the controller based on its resources.  | 
| Mode | Mode of the controller on which it is operating. | 
Driver Version  | Current version of driver installed on the system.  | 
Driver Name  | Driver name describes the name of the driver.  | 
I2C Address  | I2C address describes the Inter-Integrated Circuit(I2C) slave address.  | 
| Reboot Required Reasons | Indicates the reason why a controller cold reboot is required. | 
Rebuild Priority  | Rebuild priority determines the urgency with which the controller treats an internal command to rebuild a failed logical drive. At the low setting, normal system operations take priority over a rebuild. At the medium setting, rebuilding occurs for half of the time, and normal system operations occur for the rest of the time. At the medium high setting, rebuilding is given a higher priority over normal system operations. At the high setting, the rebuild takes precedence over all other system operations.  | 
Expand Priority  | Expand Priority setting determines the urgency with which the controller treats an internal command to expand an array. At the low setting level, normal system operations take priority over an array expansion. At the medium setting, expansion occurs for half of the time, and normal system operations occur for the rest of the time. At the high setting, the expansion takes precedence over all other system operations.  | 
Consistency Check Priority  | Consistency Check Mode is an automatic background process that ensures that you can recover data if a drive failure occurs. The scanning process checks physical drives in fault-tolerant logical drives for bad sectors and it also verifies the consistency of parity data if applicable. The available modes are disable, high, or idle. The idle mode must also specify a delay value. When set to high, the check will run in parallel to host I/O and may have an impact on performance. When set to idle, the check will only run during periods of host inactivity and will not impact performance.  | 
Consistency Check Delay  | Consistency Check Delay determines the time interval for which a controller must be inactive before a consistency check is started on the physical drives that are connected to it. The value can be between 0 and 30 to specify the duration of the delay in seconds. A value of 0 disables the scan. The default value is 3 seconds.  | 
Parallel Consistency Check Count  | Parallel consistency check count describes the number of logical devices on which the controller will perform consistency check in parallel.  | 
Consistency Check Inconsistency Notify  | Consistency Check Inconsistency Notify property enables the event notification messages and serial debug log messages for mirrored volumes.  | 
Spare Activation Mode  | Spare activation mode feature enables the controller firmware to activate a spare drive. The firmware starts rebuilding a spare drive only when a data drive fails, if the mode is set to Failure. With the predictive failure activation mode, rebuilding can begin before the drive fails when a data drive reports a predictive failure (SMART) status which will reduce the likelihood of data loss that could occur if an additional drive fails.  | 
| UEFI Health Reporting Mode | UEFI Health Reporting Mode allows the user to change whether to
                            report UEFI driver health error messages on the boot screen and halt the
                            boot process or not. The UEFI Health Reporting Mode can be either
                            “Enabled” or “Disabled”.  The default mode is “Enabled”, which reports all the UEFI driver health error messages on the boot screen and halts the boot process. The “Disabled” mode does not report any UEFI driver health error messages on the boot screen and continues the booting regardless of the errors. | 
Drive Cache  | |
Write Cache Policy for Configured Drives  | This option allows to configure the write cache policy on a controller. Setting to default allows the controller to optimize the drive write cache policy of those drives. Enabling drive write cache can increase write performance but risks losing the data in the cache on sudden power loss. Setting the policy to “unchanged” means that the controller will make no changes to the drive’s default power-on write cache policy.  | 
| Property | Tooltip Details | 
|---|---|
| Status | Status of the accelerator based on its resources. | 
| Accelerator ID | Describes the unique identifier of the accelerator. | 
| Serial Number | 
                                 A unique number assigned to the controller, used for identification and inventory purposes.  | 
| WWN | A World Wide Name (WWN) is a unique identifier of the controller. | 
| Physical Slot | PCI slot number to which the controller is connected. | 
| Temperature | Current temperature of the controller. | 
| Power Consumption | Power Consumption of the controller. | 
| Negotiated PCIe Data Rate | 
                                 Negotiated PCIe Data Rate describes the PCIe version, lane width and throughput details.  | 
| PCI Address (Domain:Bus:Device.Function) | PCI address describes the PCI address for the controller. | 
| NOR Flash Type | Describes the NOR Flash Type of the controller. | 
| Firmware Version | Active firmware version of the controller. | 
| Hardware Revision | Describes the hardware revision information about the controller. | 
| Hardware Minor Revision | Describes the hardware minor revision information about the controller. | 
| CPLD Revision | Describes the CPLD revision information about the controller. | 
Property  | Tooltip Details  | 
|---|---|
ID  | ID describes unique array identifier within the controller.  | 
Name  | Name describes unique name of array.  | 
Device Type  | Type describes the type of the array such as data array, backup array and so on.  | 
Interface Type  | Disk drives which are the member of array can have interface type such NVMe SSD. The interface type of array is based on the member disk drives interface type.  | 
Total Space  | Total usable size is the total space available in the array for creating logical device.  | 
Used Size  | The total disk space used by the logical device(s) on the given array.  | 
Unused Size  | Unused size is the free space available to create new logical device to store the data.  | 
Member Device(s) Block Size  | Block size indicates the maximum size of data block on disk drives which are member of array (can be 512 Bytes or 4K).  | 
| Status | The status of the array based on the state of its member physical device(s). | 
Transformation Status  | Transformation status indicates whether the array is transforming or not.  | 
Protected by Hot Spare  | Protected by Hot Spare indicates whether the array is protected by Hot Spare.  | 
Spare Rebuild Mode  | Spare rebuild mode describes the spare type for the array. It can be "dedicated" or "auto replace" if the array is valid.  | 
Member Logical Device(s)  | Number of logical device(s) present in the array.  | 
Member Physical Device(s)  | Number of physical device(s) used to create the array.  | 
Spare Drive(s)  | Number of spare drives associated to this array. If a drive fails in the array, the controller automatically rebuilds the data onto the spare drive.  | 
Property  | Tooltip Details  | 
|---|---|
ID  | Describes unique ID of logical device listed.  | 
RAID Level  | RAID level on which the logical device has been created.  | 
Device Type  | Drive type indicates the type of logical device, such as data and so on.  | 
Interface Type  | Disk drive which are RAID member of logical device can have interface type such as NVMe will also reflect as interface type of logical device.  | 
Data Space  | Data space is where actual data is striped across the disk drives.  | 
Stripe Size  | Stripe size is the amount of data (in KB) written to one disk drive, before moving to the next disk drive in the logical device. Stripe size options vary, depending on your controller and RAID level.  | 
Full Stripe Size  | Full stripe size refers to the combined size of all the strips across all physical drives, excluding parity-only drives.  | 
Member Device(s) Block Size  | Maximum size of data block on disk drives which are RAID member of logical device (can be 512 Bytes or 4K).  | 
Volume Unique Identifier  | The logical device unique identifier.  | 
Heads  | Heads indicates the pre-defined space set aside for RAID redundant information on a logical device.  | 
Sectors Per Track  | Sectors Per Track specifies the number of sectors that are to comprise each track.  | 
Cylinders  | Cylinders indicates the set of all of tracks of equal diameter in a logical device.  | 
Status  | The status of the logical device based on the state of its RAID members.  | 
Name  | Logical device name can be a maximum of 64 characters and it should contain only ASCII characters Note: Duplicate logical device names are not allowed.  | 
Disk Name  | Name of the logical disk drive  | 
Mounted  | Mount points describes the Operating system device names of the logical device.  | 
Protected by Hot Spare  | Protected by Hot Spare indicates whether the logical device is protected by Hot Spare.  | 
| Consistency Check Status | Indicates whether the consistency check is currently running on the logical device or not. | 
| Last Consistency Check Completion Time | Indicates when the last consistency check was completed on the logical device. | 
| Last Consistency Check Duration | Indicates how long it took to complete the last consistency check on the logical device. | 
Property  | Tooltip Details  | 
|---|---|
Vendor  | Physical device manufacturer name.  | 
Model  | Product model name of the physical device.  | 
Serial Number  | Serial number of physical device.  | 
Interface Type  | Interface type supported by the physical device.  | 
Total Size  | Total data storage capacity of the physical device.  | 
| Logical/Physical Block Size | Specifies the unit of data that can be physically read or written to the disk. Maximum size of data block on disk drives which are RAID member of logical device (can be 512 Bytes or 4K). | 
Firmware Level  | Firmware version of the physical device.  | 
Unique ID  | ID to uniquely identify the physical device.  | 
Reported Channel  | The channel to which the physical device is connected.  | 
Reported Device ID  | The unique identifier of a physical device reported by controller.  | 
| PCI Address (Domain:Bus:Device.Function) | The PCI address uniquely identifies the device, facilitating its management and configuration within the system. | 
| Parent PCI Address (Domain:Bus:Device.Function) | Uniquely identifies the device, facilitating its management and configuration within the system. | 
| XLR Configuration State | Indicates the current status of the NVMe drive, showing whether they are configured or unconfigured. | 
| Label | Used to identify each NVMe drive. | 
Sanitize Erase  | Specifies whether the sanitize erase is supported by this physical device.  | 
Encryption Capability  | Capability of drive that automatically and continuously encrypts the data on the drive without any user interaction.  | 
State  | The state of a physical drive indicates its current operational status or condition. | 
Negotiated Transfer Speed  | Negotiated data transfer rate of selected physical device.  | 
Configuration Type  | Determines the presence/type of logical devices of which this physical device is a part of.  | 
Has Stale RIS Data  | Specifies whether the physical device has stale RIS data.  | 
| SMART | Indicates whether the physical device supports SMART or not. | 
S.M.A.R.T. Warning  | Any SMART warning reported on physical device.  | 
Current Temperature  | Current temperature of the physical device.  | 
Maximum Temperature  | The maximum temperature reported by the physical device.  | 
Threshold Temperature  | The threshold temperature value of the physical device.  | 
Physical Link Rate  | Physical Link Rate  | 
Logical Link Rate  | Logical Link Rate  | 
Maximum Link Rate  | Maximum Link Rate  | 
Last Failure Reason  | Indicates last known failure occurred on this device.  | 
| Unsupported Reason | Depicts the reason for why the physical device is not supported. | 
| Power-On Hours | Indicates the number of hours the NVMe SSD has been powered on. | 
| Usage Remaining | Indicates the percentage of the NVMe SSD that has not worn out. Usage remaining is equal to the difference of 100 and the NVMe SSD Utilization percentage. | 
| Estimated Life-Remaining | Estimated Life Remaining based on workload to date indicates an estimate of the number of days the NVMe SSD has before NVMe SSD Utilization reaches 100%. | 
| Smart Trip Wear-Out | Indicates the NVMe SSD's wear status. | 
| Fifty Six Days Warning | Indicates fifty six days warning. |