7.7 Increasing the Capacity of a Logical Drive
You can add more NVMe drive space, or expand, a logical drive, to increase its capacity.
The expanded logical drive must have a capacity that is greater than or equal to the original logical drive.
Note: You can expand a logical drive only into the
        free space of the host array. To add physical drives in an array, see Modifying an Array.
To increase the capacity of a logical drive:
- In the Enterprise View, select a controller, then select the logical drive you want to expand.
 - 
        On the ribbon, in the Logical Device group, click
          Expand/Migrate. 

The Expand/Migrate Logical Device wizard opens.
 - 
        Click Expand, then click
        Next.
        

 - Enter the new logical drive size in the space provided. It must be greater than or equal to the current size.
 - Click Next.
 - Review the summary of logical drive settings. To make changes, click Back.
 - 
        Click Finish.
        The logical drive is expanded and its capacity is increased to the new size.