12.3 Recovering from a Physical Drive Failure
This section describes how to recover when an NVMe SSD fails:
- If the logical drive is protected by a hot spare, see Failed Physical Drive Protected by a Hot Spare.
 - If the logical drive is not protected by a hot spare, see Failed Physical Drive Not Protected by a Hot Spare.
 - If there is a physical drive failure in more than one logical drive simultaneously, see Failure in Multiple Logical Drives Simultaneously.
 - If it is a RAID 0 logical drive, see Physical Drive Failure in a RAID 0 Logical Drive.
 - If multiple physical drives fail within the same logical drive, see Forcing a Logical Drive with Multiple Drive Failures Back Online.