10.8 Updating the Disk Drive Firmware
Use the Firmware Update wizard to update the firmware for one or more physical drives of the same type on the local or a remote system.
To update the physical drive firmware:
- In the Enterprise View, select a system.
- On the ribbon, in the System group, click Firmware Update.

- When the wizard opens, select Disk Drive, then click
Next.

- In the Select Devices panel, select the drive to perform firmware update operation, then click Next.

- In the Flash Options panel, select the Chunk Size, from 1-n, in kilobytes (KB), then click Next.

- In the Select Files panel, click Choose, browse the file system for the firmware update file, click Open to select the file (the button label may be different on your browser).

- When the file name appears in the Uploaded Firmware Image File(s) list, click Next.
- Review the update summary, then click Finish.