7.9 Renaming a Logical Drive
- In the Enterprise View, select a controller, then select the logical drive you want to rename.
-
On the ribbon, in the Logical Device group, click Set
Properties.
The Set Properties window opens. -
In the Logical Device Name field, type the new name, then click
OK. Names can include any combination of
letters, numbers, and spaces.
maxView Storage Manager updates the logical drive name and displays the new name in the Enterprise View.
Note: Duplicate logical device names are not allowed.