11.4 Changing an Operating System's Event Log Setting

In addition to the maxView Storage Manager event log, all Warning- and Error-level events on a system are recorded in its operating system event log. You can select the type of events that are recorded, or you can disable operating system event logging.

To change or disable operating system event logging on a system:

  1. Select the Enterprise View node.
  2. On the ribbon, in the System group, click System Settings.

    The System Settings window opens.

  3. In the Save Events to OS Log drop-down list, select the type of events that you want to log, then click OK.
  4. Restart maxView Storage Manager to apply the new setting.