7.5 Modifying an Array
maxView Storage Manager allows you add Drives to an Array. If you add the logical drives, you are expanding the array by adding the data drives.
To add drives in an array:
- In the Enterprise View, select an array.
-
On the ribbon, in the Array group, click Modify Array.

-
When the wizard opens, select Add Drive(s), then click
Next.

-
If you are adding the new drives to an array, select the physical drives for the array.
Be sure the drive type is the same for all drives.
Note: The drives must have sufficient capacity to store the logical drive data. - Click Next, review the summary information, then click Finish.