7.5 Modifying an Array

maxView Storage Manager allows you add Drives to an Array. If you add the logical drives, you are expanding the array by adding the data drives.

To add drives in an array:

  1. In the Enterprise View, select an array.
  2. On the ribbon, in the Array group, click Modify Array.
  3. When the wizard opens, select Add Drive(s), then click Next.
  4. If you are adding the new drives to an array, select the physical drives for the array. Be sure the drive type is the same for all drives.
    Note: The drives must have sufficient capacity to store the logical drive data. For optimal performance, use the physical device(s) that are attached to the same NUMA node. The selection of physical device(s) that are attached to different NUMA nodes may impact performance.
  5. Click Next, review the summary information, then click Finish.