8.6 Creating Logical Device
This section explains how to create a logical device using SED drives. Mixing of drives to create the logical device is not allowed, for example; mixing of block sizes (512 Bytes and 4K) and SED types (Opal and Enterprise). To create a logical device, the SED drive must be either in OFS or the ownership status should be MCHP Owned.
Additional device types with the following combination are listed along with the other device type in the Create Logical Device window only when the SED based encryption is configured/enabled.
- NVMe SED Opal SSD 512
- NVMe SED Enterprise SSD 512
- NVMe SED Opal SSD 4K
- NVMe SED Enterprise SSD 4K
Once the SED based encryption is configured, on the RAID Members tab, the Device Type dropdown will have the extra device type(s). Select the SED drives and click Next.

On the RAID Attributes tab, select the Encrypt Data check box to encrypt the array and logical device; else it will create the plaintext logical device.