6.13 Frame transmitted despite confirmed transmit cancellation for CAN-FD messages with more than 8 data bytes
In case the transmission of Tx Buffer nn was not successful and is restarted immediately afterwards by automatic retransmission, and the software requests a Tx cancellation for this Tx Buffer by setting the cancellation request bit MCAN_TXBCR.CRnn during transmission of the first 4 identifier bits, a successful cancellation is incorrectly signalled by setting MCAN_TXBCF.CFnn = ’1’ and by clearing MCAN_TXBRP.TRPnn. In addition, the respective Transmission Occurred bit remains zero (MCAN_TXBTO.TOnn = ’0’), incorrectly indicating that the frame was not transmitted on the bus.
Other than signalled by MCAN_TXBCF.CFnn and MCAN_TXBTO.TOnn, the transmission continues until the complete frame has been sent on the CAN bus. If the transmission is successful, MCAN_TXBTO.TOnn will be set.
If in this case new data is written to Tx Buffer nn while the transmission is still ongoing, a frame with inconsistent data may appear on the bus.
This problem is limited to the case of transmit cancellation of CAN-FD messages with more than 8 data bytes while automatic retransmission is enabled (MCAN_CCCR.DAR = ’0’).
Transmit cancellation of Classical CAN messages and CAN-FD messages with up to 8 data bytes is not affected.
CAN 2.0 operation is not impacted.
Work around
Do not use transmit cancellation for CAN-FD messages with more than 8 data bytes.
Alternatively, wait for the duration of the expected transmission time of the cancelled Tx Buffer before writing new data to that Tx Buffer.
Affected Silicon Revisions
| A | B | C | |||||
| X | X | X |