2 Schematic checklist:

This section provides a general checklist for touch applications. For application-specific information, please refer to the relevant topics or contact the Microchip Technical Support team.

  • Place Bulk and Decoupling capacitors as recommended in the datasheet.
  • Add series resistor to the touch drive pins, sense pins and the driven shield pin.
  • Use a resistance value between 1 kΩ and 100 kΩ for the touch lines.
  • The resistance value of the driven shield should be one-tenth of the resistance value used for the touch line
  • Define the state of the LED driven pin as either VCC or GND, depending on the design of the LED circuits.