2.5 Creating a New MCC Harmony Project

Figure 2-20. MPLAB X IDE Start-up Screen
  1. To create a new project, open MPLAB X IDE and click on File>New Project
    Figure 2-21. New Project
  2. In the “New Project” pop-up, click on Microchip Embedded>Application Project(s)>Next
    Figure 2-22. Choose Project
  3. In Select Device window, select the device from drop down and click Next.
    Figure 2-23. Select Device
  4. In Select Compiler window, Select the latest compiler and click Next.
    Figure 2-24. Select Compiler
  5. In Select Project Name and Folder window, enter the project name and select the project location, and click Finish.
    Figure 2-25. Select Project Name and Folder
  6. Locate the Harmony Framework path and click Next
  7. Now MPLAB X Code Configurator Content Manager will be launched automatically.
    1. Click on Finish
      Figure 2-26. MCC Required Content
    2. Project Graph window of the Configurator may have predefined components.
      Figure 2-27. Project Graph
    3. Project and Device resources
      Figure 2-28. Project and Device resources