This section describes in detail on how to install the correct versions of the required Harmony 3
component dependencies. The following table summarizes the components and versions that will
be installed.
Table 2-3. Harmony Components
Harmony components to be cloned with MCC Content Manager
Version
csp
3.18.0
core
3.13.0
dev_packs
3.17.0
bsp
3.17.0
CMSIS-FreeRTOS
10.3.1
crypto
3.8.0
wolfssl
4.8.1
Zlib
1.2.13
wireless_ble
1.1.0
wireless_system_pic32cxbz_wbz
1.3.0
wireless_apps_pic32cxbz2_wbz45
3.0.0
wireless_pic32cxbz_wbz
1.2.0
wireless_zigbee
5.1.1
Cloning Harmony Repositories using MCC Content
Manager Wizard
Create a new “MCC Harmony” project (Create an empty project and clone the required repositories
to clone the Harmony repositories)
In MPLAB X IDE, select New ProjectFigure 2-5. New Project Creation
In the New Project tab, select 32-bit MCC
Harmony ProjectFigure 2-6. MCC Harmony Project
option.
Framework Selection (Local PC directory where
cloned repos are placed)Figure 2-7. Framework Selection
In the New Project tab, select the project settings and the correct Project
Folder Path and Name Selection.Figure 2-8. Project Settings
In Configuration Settings, select the
device WBZ451.
Figure 2-9. Configuration Settings
Open MPLAB Code Configurator
after creating the project. MCC Content Manager window appears in IDE.
Figure 2-10. MCC
in IDE.
In the Content Manager Wizard Window, select MPLAB Harmony. Figure 2-11. MCC Content Manager Window
Select Optional Content as illustrated in the following figure. Figure 2-12. Optional Content Window
MCC
Ensure all components are selected as displayed
in the following image. Ignore version selection for now, as it will be taken care at a
later stage. Figure 2-13. Required Content
Select Finish. The downloading of
selected components from harmony repositories will take some minutes. If all the selected
components are cloned successfully, MCC logs in IDE will display the following
information.
Figure 2-14. MCC Logs Snapshot when all
selected components are cloned successfully
Attention
If in the
process a failure to download a particular component appears, try
redownloading again only the component that failed to download. For example,
if user received a prompt from MCC saying “dev_packs” was not
download
close the MCC reopen
MCC again and start from step 3 in this section, with the “dev_packs” as the
only missing component for downloading and select “Finish”
Figure 2-17. Framework Selection PathProject Graph Window appears after choosing the framework path and successful
initialization of the project. Figure 2-18. Project Graph
Change to content versions recommended for use during development in the table. In the Content
Manager tab, of the Device Resources, select Apply. This step is important and
must be followed by the user as every wireless stack and app example release is tested with
certain version of dependent component.Figure 2-19. Changing content versions
After successfully checking out the right version of content/components, for more details on
developing an application, refer to start developing application
examples.