3.2.5 BLE Proximity Reporter
Introduction
The Proximity Reporter application provides comprehensive guidance on setting up, programming, and testing a BLE Proximity Reporter using the WBZ451 Curiosity board. This document details the necessary hardware and software requirements, the Bluetooth Low Energy (BLE) proximity profile, and specific services involved. It also includes step-by-step instructions and test scenarios for implementing and validating the application.
Hardware Requirement
Tool |
Quantity |
---|---|
WBZ451 Curiosity Board |
1 |
Micro USB Cable |
1 |
Mobile |
1 (Smart phone with the Microchip Bluetooth Data (MBD) app installed) |
Software Requirements
- MPLABX IPE: For programming the precompiled hex file.
- MPLABX IDE: For programming the application example.
Programming the Precompiled Hex File or Application Example
Programming the .hex
File using MPLAB X IPE
- Precompiled
.hex
file is located in<Harmony Content Path>\wireless_apps_pic32cxbz2_wbz45\apps\ble\advanced_applications\ ble_pxpr_app\firmware\ble_pxpr_app.X\dist\default\production
folder. - For more details on the steps, go to
Programming A Device Note: Ensure to choose the correct Device and Tool information.
Programming the Application using MPLAB X IDE
- Follow the steps mentioned in Running a Precompiled Example section.
- Open and program the application example
“
ble_pxpr_app.X
” located in<Harmony Content Path>\wireless_apps_pic32cxbz2_wbz45\apps\ble\advanced_applications\ble_pxpr_app\firmware\ble_pxpr_app.X
using MPLAB X IDE.
For more details on finding the Harmony content path, refer to Installing the MCC Plugin
Proximity Profile
In the context of Bluetooth Low Energy (BLE), “proximity” generally refers to the physical closeness between two BLE devices. The BLE Proximity profile is a standardized BLE profile that enables a device to alert a user when another device is near or far away from it.
The Proximity profile defines the behavior when a device moves away from a peer device so that the connection is dropped or the path loss increases above a preset level, causing an immediate alert. This alert can be used to notify the user that the devices have become separated.
- Proximity Reporter (Server): This refers to the tracked device, which could be an item like a key fob or any other asset whose proximity is to be monitored
- Proximity Monitor (Client): This device monitors the reporter's proximity, typically through a smart phone or tablet
The Proximity profile uses the RSSI (Received Signal Strength Indicator) to determine the approximate distance between the Monitor and the Reporter.
Role/Service Relationships
The following figure shows the relationship between services and the two profile roles. The
dotted line indicates that the service within this line is optional.
Proximity Reporter Requirements
The Proximity Reporter must have one instance of the Link Loss Service and may have instances of both the Immediate Alert Service and the Tx Power Service. these services are described in detail below:
Link Loss Service
Link loss service in Bluetooth Low Energy (BLE) is a standard service defined by the Bluetooth Special Interest Group (SIG) to alert a device when it loses connection with another device.
- The Link Loss Service uses the Alert Level characteristic to cause an alert in the device when the link is lost.
- The Link Loss Service can be
instantiated as a “Primary Service”. The service UUID can be set to the UUID value
assigned to “Link Loss” which is
0x1803
.
Service Characteristics
The Alert Level Characteristic is used to expose the current link loss alert level that is used to determine how the device alerts when the link is lost.
Characteristic |
Mandatory/Optional |
Characteristics Property |
---|---|---|
Alert Level |
Mandatory |
Read, Write |
Characteristic Behavior
The Alert Level characteristic can be set to “No Alert,” “Mild Alert,” “High Alert”.
Service Behaviors
Disconnection Behavior
- No Alert: alter will be disabled
- Mild Alert: triggers the mild alert
- High Alert: this will trigger the strongest possible alert
The specific action that occurs in the device for the mild and high alerts is implementation specific. For example, this could include flashing lights, making noises, moving, or other methods to alert the user.
- An implementation-specific timeout
- User interaction on this device
- The physical link is reconnected
Immediate Alert Service
This service exposes a control point to allow a peer device to cause the device to alert immediately. The proximity monitor will calculate the path loss:
Path Loss = Tx Power Level - RSSI
If the path loss exceeds a certain threshold, the monitor can write the alert level characteristic of the IAS, thereby prompting the user to perform appropriate action to avoid disconnection.
The alert level characteristic can be written using the GATT Write without Response sub-procedure with an alert level of “No Alert,” “Mild Alert,” “High Alert,” to set the written alert level.
Characteristic |
Mandatory/Optional |
Characteristics Property |
---|---|---|
Alert Level |
Mandatory |
Write, Without Response |
- No Alert: alter will be disabled
- Mild Alert: triggers the mild alert
- High Alert: this will trigger the strongest possible alert
The specific action that occurs in the device for the mild and high alerts is implementation specific. For example, this could include flashing lights, making noises, moving, or other methods to alert the user.
Tx Power Service
The Tx Power Service uses the Tx power level characteristic to expose the current transmit power level of a device when in a connection.
Characteristic |
Mandatory/Optional |
Characteristics Property |
---|---|---|
Tx Power Level |
Mandatory |
Read |
The Tx Power Level characteristic returns the current transmit power level when read using the GATT Characteristic Read.
Proximity Reporter Application
In this section, the focus is on the Proximity Reporter application implementation specific details. In terms of the application design and testing methods.
Project Graph
The components illustrated in the project graph is used to create the Proximity Reporter application.
The MCC supports the proximity profile and associated services like Immediate Alert Service, Link Loss Service and Tx Power Service. And the other mandatory components listed below is also available as a drag and drop components in the MCC.
Working Flow
APP_PXPR_STATE_IDLE
: application remains in the Idle mode.APP_PXPR_STATE_ADV
: application is waiting for a connection without bond within timeout_adv seconds duration.APP_PXPR_STATE_BOND_ADV
: application is waiting for a reconnection with bond within timeout_with_bond_adv seconds duration.APP_PXPR_STATE_CONN
: application is prepared to respond to Proximity Monitor role.
Input and Output Interface
Input
The application relies on Button 1 as the input.
- Types of Pressing:
- Press: Press the button for less than 500 ms.
- Long press: Press the button for more than 500 ms.
- Application behavior on button press in different state co relation.
State |
Action |
Behavior |
---|---|---|
|
Long press Button 1 |
Disconnect the existing connection, enable advertisement and allow new device to be bonded |
|
Long press Button 1 |
Enable advertisement and allow new device to be bonded |
Output
- Current application state: The RGB LED (blue) is used
- Alert state: User LED (blue) is used
APP Connection State |
LED Behavior |
---|---|
APP_PXPR_STATE_IDLE |
All LEDs are turned OFF. |
APP_PXPR_STATE_ADV |
The RGB LED (blue) flashes once every 3 seconds. (ON: 50 ms, OFF: 2950 ms) |
APP_PXPR_STATE_BOND_ADV |
The RGB LED (blue) flashes twice every 3 seconds. (ON: 50 ms, OFF: 50 ms) |
APP_PXPR_STATE_CONN |
The RGB LED (blue) flashes twice every 1.5 seconds. (ON: 50 ms, OFF: 150 ms) |
The User LED pattern indicates the alert state according to the following table:
APP Alert Level |
LED Behavior |
---|---|
|
User LED (Blue) remains ON |
|
User LED (Blue) blinks once every second |
|
User LED (Blue) blinks five times every second |
Test Cases
The test case section covers separate test scenarios to test the Link Loss, Immediate Alert Services and Tx Power Service behavior implementation.
- Mobile Application
In this testing, Android mobile is taken for demonstration with Microchip Bluetooth Data (MBD) mobile application installed
- Windows system
- WBZ451 Curiosity board as the development board. Connected to Windows machine using a USB cable.
- MPLAB X IDE
Link Loss
The below session covers the test case scenarios that showcase the Link Loss Service. The Link Loss Service provides provision to set the desired alert level using the alert level characteristic to cause an alert in the device when the link is lost. Based on the set alert level, the indication will be displayed on the Proximity Reporter on the event of disconnection.
The test case covers:
- How to use the mobile (Android) MBD application to establish the connection with PXPR curiosity board.
- Link Loss Service Alert level configuration.
- Testing scenarios to observe LED behavior during the disconnection.
- In the MPLABX, open the
ble_pxpr_app
(Reporter) application. Compile and program the PXPR application on the Curiosity board with the below configuration.Table 3-43 3-46 3-49 3-51 3-52. Version Details PIC32CX-BZ2_DFP
1.3.238
XC32 Compiler Version:
V4.40
-
After programming (or resetting) the device will be in
APP_PXPR_STATE_ADV
. -
APP_PXPR_STATE_ADV
: The application is waiting for a connection without bond. That too within timeout_adv_seconds (60 seconds). After the completion of the timeout the device entersAPP_PXPR_STATE_IDLE
state.timeout_adv = 60 seconds - Timeout for advertisement without bond.
LED Behavior
APP_PXPR_STATE_ADV
= RGB LED (blue) flashes once in every 3 seconds.APP_PXPR_STATE_IDLE
= RGB LED (blue) will turn OFF.
-
- Open the Microchip Bluetooth Data (MBD) app in Android and click BLE Connect feature.
- Click START SCAN icon to see the
nearby advertising devices. From the list of devices PXPR is the target device.
Figure 3-241. BLE Scanner - Click PXPR device to establish the
connection. All the supported profiles in the proximity reporter will be displayed upon
connection. At the peripheral side, the PXPR curiosity board will
enter
APP_PXPR_STATE_CONN
when the connection is established.The on-board RGB LED (blue) indicate the connection and advertisement state as follows.
Table 3-44. Application State APP State LED Behavior APP_PXPR_STATE_IDLE
All LEDs are turned OFF.
APP_PXPR_STATE_ADV
The RGB LED (blue) flashes once every 3 seconds. (ON: 50 ms, OFF: 2950 ms)
APP_PXPR_STATE_CONN
The RGB LED (blue) flashes twice every 1.5 seconds. (ON: 50 ms, OFF: 150 ms)
- On the MBD app, press the Link Loss
Service icon.
Figure 3-242. Link Loss Service - Select the desired Alert Level from the
available option (No Alert, Mild Alert, High Alert).
- Press the “←” icon on the top left corner
of the screen twice to disconnect the “PXPR”. The Link Loss Service alert level will be
shown as
BLE_PXPR_ALERT_LEVEL_HIGH
and can be observed through the PXPR User LED LED.Table 3-42 3-45 3-47 3-50. APP Alert Level APP Alert Level
LED Behavior
BLE_PXPR_ALERT_LEVEL_NO
User LED (Blue) remains ON
BLE_PXPR_ALERT_LEVEL_MILD
User LED (Blue) blinks once every second
BLE_PXPR_ALERT_LEVEL_HIGH
User LED (Blue) blinks five times every second
Immediate Alert Test case
The following session covers the test case scenarios that showcase the Immediate Alert Service usage. The usage includes how to set the range for different zone and what all alert level can be set in each zone so that the preset alert indication will be displayed on Proximity Reporter (Curiosity board) based on the distance between Proximity Monitor (Mobile) and Reporter.
Separate test cases are derived to showcase the application behavior with and without encryption and power control. The encryption feature will establish a paired connection and the power control. Disabling option excludes the auto adjust TX power configuration (based on the range) by the BLE firmware.
The test case covers:
- How to use the mobile (Android) MBD application to establish the connection with PXPR Curiosity board.
- Immediate Alert Service Range Bar configuration.
- Alert level configurations on each zone.
- Testing scenarios to observe LED behavior in each alert level in different distance range.
- Test Case 1: Without Encryption and Power Control
This test case is based on a non-secure connection without encryption and power control features.
- In the MPLAB X, open the
ble_pxpr_app
(Reporter) application. Compile and program the PXPR application on the Curiosity board with the below configuration.Table 3-43 3-46 3-49 3-51 3-52. Version Details PIC32CX-BZ2_DFP
1.3.238
XC32 Compiler Version:
V4.40
-
After programming (or resetting), the Proximity Reporter application will be in
APP_PXPR_STATE_ADV
state. APP_PXPR_STATE_ADV
: The application is waiting for a connection without bond. Duration withintimeout_adv_seconds
(60 seconds). After the completion of the timeout the device entersAPP_PXPR_STATE_IDLE
state.Note:timeout_adv
= 60 seconds - Timeout for advertisement without bondLED Behavior:
APP_PXPR_STATE_ADV
: RGB LED (blue) flashes once in every 3 secondsAPP_PXPR_STATE_IDLE
: RGB LED (blue) will turn OFF
-
- Open the Microchip Bluetooth Data (MBD) app in Android and click BLE Connect feature
- Click START SCAN icon to see
the nearby advertising devices. From the list of devices PXPR is the target
device
Figure 3-243. BLE Scanner - Click PXPR device to establish
the connection. All the supported profiles in the proximity reporter will be displayed
upon connection. At the peripheral side, the PXPR curiosity board will
enter
APP_PXPR_STATE_CONN
when the connection is established. - Click Immediate Alert Service
icon as illustrated below.
Figure 3-244. Immediate Alert Service - Press the setting icon (Highlighted
in green border) in the top right corner of the screen to configure the link budget
threshold set to a proper value. It is based on the range bar value configuration in
which the zone distance is calculated.
Figure 3-245. Configuring Link Budget Threshold - The colored circles (Green, Orange, Red) shows the range for SAFE, MID, DANGER
zone. The real time distance covered in each zone is user configurable. The
configuration can be done in the range bar. The following figure illustrates the
range bar configuration.
Figure 3-246. Range Bar
- The colored circles (Green, Orange, Red) shows the range for SAFE, MID, DANGER
zone. The real time distance covered in each zone is user configurable. The
configuration can be done in the range bar. The following figure illustrates the
range bar configuration.
- The alert level at the PXPR
(Curiosity board) which is based on the distance to the central device (Mobile) is
user-configurable on the Immediate Alert Service settings page. User can configure for the alert level required for each zone. In The SAFE, MID, DANGER region are set as per the user configuration in the Range Bar.
Figure 3-247. Alert Configuration -
The on-board User LED shows the indication based on the alert level set at each zone. As per the above configuration, when the mobile is near the Proximity Reporter (PXPR), the alert level will be
BLE_PXPR_ALERT_LEVEL_NO
. When the mobile phone moves away then the alert level will beBLE_PXPR_ALERT_LEVEL_MILD
. If the Proximity Reporter (PXPR) moves further away the alert level will beBLE_PXPR_ALERT_LEVEL_HIGH
.The LED behavior in each level will be as per the following table.
Table 3-42 3-45 3-47 3-50. APP Alert Level APP Alert Level
LED Behavior
BLE_PXPR_ALERT_LEVEL_NO
User LED (Blue) remains ON
BLE_PXPR_ALERT_LEVEL_MILD
User LED (Blue) blinks once every second
BLE_PXPR_ALERT_LEVEL_HIGH
User LED (Blue) blinks five times every second
The RGB LED (blue) patterns to indicate the current application state according to the following table:Table 3-41 3-48 3-53. APP Connection State and Behavior APP Connection State
LED Behavior
APP_PXPR_STATE_IDLE
All LEDs are turned OFF.
APP_PXPR_STATE_ADV
The RGB LED (blue) flashes once every 3 seconds. (ON: 50 ms, OFF: 2950 ms)
APP_PXPR_STATE_BOND_ADV
The RGB LED (blue) flashes twice every 3 seconds. (ON: 50 ms, OFF: 50 ms)
APP_PXPR_STATE_CONN
The RGB LED (blue) flashes twice every 1.5 seconds. (ON: 50 ms, OFF: 150 ms)
- In the MPLAB X, open the
-
Test 2: With Encryption and Power Control
This test case demonstrates the feature tested with security connection with encryption and power control features.
- In the MPLAB X, open the
ble_pxpr_app
(Reporter) application. Compile and program the PXPR application on the Curiosity board with the below configuration:- Uncomment the compile option
BLE_PXPR_LLS_AUTH_ENABLE
inble_lls.c
- Uncomment the compile option
BLE_PXPR_IAS_AUTH_ENABLE
inble_ias.c
- Uncomment the compile option
POWER_CTRL_ENABLE
ininitialization.c
Table 3-43 3-46 3-49 3-51 3-52. Version Details PIC32CX-BZ2_DFP
1.3.238
XC32 Compiler Version:
V4.40
- After programming (or resetting) the device will be in
APP_PXPR_STATE_ADV
state. -
APP_PXPR_STATE_ADV
: The application is waiting for a connection without bond. Duration withintimeout_adv_seconds
. After the completion of the timeout the device enters intoAPP_PXPR_STATE_IDLE
state.Note:timeout_adv
= 60 seconds - Timeout for advertisement without bond.
LED Behavior:
APP_PXPR_STATE_ADV
: Green LED flashes once in every 3 secondsAPP_PXPR_STATE_IDLE
: Green LED will turn OFF - Uncomment the compile option
- Open the Microchip Bluetooth Data (MBD) app in Android and click BLE Connect feature.
- Click START SCAN icon to see
the nearby advertising devices. From the list of devices PXPR is the target
device.
Figure 3-248. BLE Scanner - Click PXPR device to establish
the connection. All the supported profiles in the Proximity Reporter will be displayed
upon connection. At the peripheral side, the PXPR Curiosity board will
enter
APP_PXPR_STATE_CONN
when the connection is established. - In the MBD app, press the Link
Loss Service icon and select the alert level
as
BLE_PXPR_ALERT_LEVEL_HIGH
/BLE_PXPR_ALERT_LEVEL_MILD
. - Notification for paring permission
will appear, click Pair button to trigger the pairing flow.
Figure 3-249. Pairing Request - On the MBD app, press the “←” icon on the top left corner of the screen and press the Immediate Alert Service icon.
- Based on the configuration made on
the settings page of Immediate Alert Service the alert level will be indicated on the
device.
Figure 3-250. Range Bar When the mobile is near the Proximity Reporter (PXPR), the alert level will be
BLE_PXPR_ALERT_LEVEL_NO
. When the mobile phone moves away then the alert level will beBLE_PXPR_ALERT_LEVEL_MILD
. If the Proximity Reporter (PXPR) moves further away the alert level will beBLE_PXPR_ALERT_LEVEL_HIGH
.Table 3-42 3-45 3-47 3-50. APP Alert Level APP Alert Level
LED Behavior
BLE_PXPR_ALERT_LEVEL_NO
User LED (Blue) remains ON
BLE_PXPR_ALERT_LEVEL_MILD
User LED (Blue) blinks once every second
BLE_PXPR_ALERT_LEVEL_HIGH
User LED (Blue) blinks five times every second
- Keep moving away from Proximity
Reporter (PXPR) until it is disconnected. The PXPR
enters
APP_PXPR_STATE_ADV_BOND
. The Link Loss Service alert level will be shown as what is set on “Link Loss Service”, which can be observed through the PXPR User LED.
- In the MPLAB X, open the
TX Power Service
The following session covers the test case scenarios that showcase the Tx Power Service. The TX Power Service uses the power level characteristic to return the current transmit power level when read using the GATT characteristic read.
The test case covers:
- How to use the mobile (Android) MBD application to establish the connection with PXPR Curiosity board.
- Read the Tx power level using the Tx Power service.
- In the MPLAB X, open the
ble_pxpr_app
(Reporter) application. Compile and program the PXPR application on the curiosity board with the below configuration.Table 3-43 3-46 3-49 3-51 3-52. Version Details PIC32CX-BZ2_DFP
1.3.238
XC32 Compiler Version:
V4.40
- In the MPLAB X, open the
ble_pxpr_app
(Reporter) application. Compile and program the PXPR application on the Curiosity board with the below configuration:- Uncomment the compile option
BLE_PXPR_LLS_AUTH_ENABLE
inble_lls.c
- Uncomment the compile option
BLE_PXPR_IAS_AUTH_ENABLE
inble_ias.c
- Uncomment the compile option
POWER_CTRL_ENABLE
ininitialization.c
Table 3-43 3-46 3-49 3-51 3-52. Version Details PIC32CX-BZ2_DFP
1.3.238
XC32 Compiler Version:
V4.40
- After programming (or resetting) the device will be in
APP_PXPR_STATE_ADV
state. -
APP_PXPR_STATE_ADV
: The application is waiting for a connection without bond. Duration withintimeout_adv_seconds
. After the completion of the timeout the device enters intoAPP_PXPR_STATE_IDLE
state.Note:timeout_adv
= 60 seconds - Timeout for advertisement without bond
LED Behavior:
APP_PXPR_STATE_ADV
: Green LED flashes once in every 3 secondsAPP_PXPR_STATE_IDLE
: Green LED will turn OFF - Uncomment the compile option
- Open the Microchip Bluetooth Data (MBD) app in Android and click BLE Connect feature.
- Click START SCAN icon to see the
nearby advertising devices. From the list of devices PXPR is the target device.
Figure 3-251. BLE Scanner - Click PXPR device to establish the
connection. All the supported profiles in the Proximity Reporter will be displayed upon
connection. At the peripheral side, the PXPR Curiosity board will
enter
APP_PXPR_STATE_CONN
when the connection is established.The on-board RGB LED (blue) LED indicate the connection and advertisement state as following.
Table 3-41 3-48 3-53. APP Connection State and Behavior APP Connection State
LED Behavior
APP_PXPR_STATE_IDLE
All LEDs are turned OFF.
APP_PXPR_STATE_ADV
The RGB LED (blue) flashes once every 3 seconds. (ON: 50 ms, OFF: 2950 ms)
APP_PXPR_STATE_BOND_ADV
The RGB LED (blue) flashes twice every 3 seconds. (ON: 50 ms, OFF: 50 ms)
APP_PXPR_STATE_CONN
The RGB LED (blue) flashes twice every 1.5 seconds. (ON: 50 ms, OFF: 150 ms)
- In the MBD app, press the Tx Power
Service icon.
Figure 3-252. TX Power Service - The highlighted portion shows the read Tx
power level.
Figure 3-253. TX Power Level